| ISS 208MM.2/L-2E0-S8.3 |
| Vendor ID |
338 (0x0152) |
 |
| Vendor Name |
Leuze electronic GmbH + Co. KG |
| Vendor Text |
The Sensor People |
| Vendor URL |
https://www.leuze.com/ |
| Device ID |
1 (0x000001) |
| DeviceFamily |
Inductive sensors |
| Features |
| Block Parameter |
yes |
| Data Storage |
yes |
| Profile Characteristic |
0x4000 (Common Application Profile: Identification and Diagnosis) |
| Communication |
| IO-Link Revision |
V1.1 |
| Transmission Rate | 38400 bit/s (COM2) |
| Minimum Cycle Time |
10.4 ms |
| SIO Mode Supported |
yes |
| M-Sequence Capability | PREOPERATE = TYPE_1_2 with 2 octets on-request data OPERATE = TYPE_2_1 with 1 octet on-request data ISDU supported |
| Device Variant |
ISS 208MM.2/L-2E0-S8.3 |
| Description |
Inductive Proximity Sensor, M8 thread, embedded, M8 connector (3 pins) |
| Product ID |
50151545 |
| Device Icon |
 |
| Device Symbol |
 |
| Connection Type | Non-standard connector |
| Connection Symbol |
 |
| Connection Description |
Sensor is connected 4-pin M12 connector |
| - pin 1 |
brown; L+; Power supply (+) |
| - pin 3 |
(light) blue; L-; Power supply (-) |
| - pin 4 |
black; C/Q; Out/IO-Link |
| subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
| 1 |
120 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
| 2 |
112 |
8-bit UInteger |
|
|
ro |
|
|
Master Cycle Time |
Communication: Current communication cycle duration used by the master. This value defines the process data cycle. |
| 3 |
104 |
8-bit UInteger |
|
|
ro |
|
|
Min Cycle Time |
Communication: Minimum communication cycle duration supported by the device. This value defines the lowest possible process data cycle. |
| 4 |
96 |
8-bit UInteger |
|
|
ro |
|
|
M-Sequence Capability |
Communication: Information on the structure and the supported features of the communication messages. |
| 5 |
88 |
8-bit UInteger |
|
17 |
ro |
|
|
IO-Link Revision ID |
Communication: Identifier for the currently used communication protocol revision. |
| 6 |
80 |
8-bit UInteger |
|
|
ro |
|
|
Process Data Input Length |
Communication: Information on width and features of the process input data (Process Data from Device to Master). |
| 7 |
72 |
8-bit UInteger |
|
|
ro |
|
|
Process Data Output Length |
Communication: Information on width of the process output data (Process Data from Master to Device). |
| 8 |
64 |
8-bit UInteger |
|
|
ro |
|
|
Vendor ID 1 |
Identification: Highest octet of the Vendor ID. Combined with the parameter Vendor ID 2, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community. |
| 9 |
56 |
8-bit UInteger |
|
|
ro |
|
|
Vendor ID 2 |
Identification: Lowest octet of the Vendor ID. Combined with the parameter Vendor ID 1, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community. |
| 10 |
48 |
8-bit UInteger |
|
|
ro |
|
|
Device ID 1 |
Identification: Highest octet of the Device ID. Combined with the parameters Device ID 2 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID. |
| 11 |
40 |
8-bit UInteger |
|
|
ro |
|
|
Device ID 2 |
Identification: Middle octet of the Device ID. Combined with the parameters Device ID 1 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID. |
| 12 |
32 |
8-bit UInteger |
|
|
ro |
|
|
Device ID 3 |
Identification: Lowest octet of the Device ID. Combined with the parameters Device ID 1 and 2, this parameter defines the 24-bit value of the vendor-specific Device ID. |
| 13 |
24 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
| 14 |
16 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
| 15 |
8 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
| 16 |
0 |
8-bit UInteger |
|
|
wo |
X |
|
System Command |
Application: Command interface for devices without ISDU support. Validity and execution of commands are not confirmed. |
| subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
| 1 |
0 |
4-bit UInteger |
0 = Idle, 1 = SP1 success, 2 = SP2 success, 3 = SP1, SP2 success, 4 = Wait for command, 5 = Busy, 7 = Error |
0 |
|
|
|
State |
Indicates the current state of the teach procedure. |
| 2 |
4 |
Boolean |
false = Initial or not ok, true = Ok |
false |
|
|
|
Flag SP1 TP1 |
Indicates the current teach result for the teach point. |
| 3 |
5 |
Boolean |
false = Initial or not ok, true = Ok |
false |
|
|
|
Flag SP1 TP2 |
Indicates the current teach result for the teach point. |
| 4 |
6 |
Boolean |
false = Initial or not ok, true = Ok |
false |
|
|
|
Flag SP2 TP1 |
Indicates the current teach result for the teach point. |
| 5 |
7 |
Boolean |
false = Initial or not ok, true = Ok |
false |
|
|
|
Flag SP2 TP2 |
Indicates the current teach result for the teach point. |
| subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
| 1 |
40 |
8-bit UInteger |
0 = High active, 1 = Low active |
0 |
|
|
|
Logic |
Defines the logical representation of the switching signal SSC in the process data. |
| 2 |
32 |
8-bit UInteger |
0 = Deactivated, 1 = Single point, 2 = Window, 3 = Two point |
1 |
|
|
|
Mode |
Defines the evaluation mode for the switching signal SSC. |
| 3 |
0 |
32-bit Integer |
0 = Default, 1 = Extended |
0 |
|
|
|
Hysteresis |
Defines the hysteresis at the switchpoint. A higher hysteresis may help to increase stability in critical applications. |
| subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
| 1 |
40 |
8-bit UInteger |
0 = High active, 1 = Low active |
0 |
|
|
|
Logic |
Defines the logical representation of the switching signal SSC in the process data. |
| 2 |
32 |
8-bit UInteger |
0 = Deactivated, 1 = Single point, 2 = Window, 3 = Two point |
1 |
|
|
|
Mode |
Defines the evaluation mode for the switching signal SSC. |
| 3 |
0 |
32-bit Integer |
0 = Default, 1 = Extended, 2..7000 |
10 |
|
|
|
Hysteresis |
Defines the hysteresis at the switchpoint. A higher hysteresis may help to increase stability in critical applications. |
| subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
| 1 |
72 |
8-bit UInteger |
0 = Disabled, 1 = PNP, 2 = NPN, 3 = Push-Pull |
3 |
|
|
|
Output Stage Mode |
|
| 2 |
64 |
8-bit UInteger |
1 = SSC1, 2 = SSC2, 5 = TA |
1 |
|
|
|
Source |
|
| 3 |
56 |
8-bit UInteger |
0 = Disabled, 1 = T-on Delay, 2 = T-off Delay, 3 = T-on and T-off Delay, 4 = One Shot Leading Edge, 5 = One Shot Trailing Edge |
0 |
|
|
|
Timer Mode |
|
| 4 |
48 |
8-bit UInteger |
0 = Milliseconds, 1 = Seconds, 2 = Minutes |
0 |
|
|
|
Timer Scale |
|
| 5 |
32 |
16-bit Integer |
1..32767 |
100 |
|
|
|
Delay Duration |
|
| 6 |
16 |
16-bit Integer |
1..32767 |
1 |
|
|
|
Divider |
|
| 7 |
8 |
8-bit UInteger |
|
|
|
|
|
Reserved |
|
| 8 |
0 |
8-bit UInteger |
0 = Normally Open, 1 = Normally Closed |
0 |
|
|
|
NO/NC Operation |
|
| Parameters Menu |
| Service Functions |
V_SystemCommand, Button:=129 Description=The parameters of the technology-specific application are set to default values. Identification parameters remain unchanged. An upload to the data storage of the master will be executed, if activated in the port configuration of the master. |
V_SystemCommand, Button:=131 Description=The parameters of the device are set to factory default values and communication will be inhibited until the next power cycle. Note: Directly detach the device from the master port! |
|
| Switching Signal Channel 1 |
| V_SSP_SSC01_Param.SP1 |
| V_SSP_SSC01_Param.SP2 |
| V_SSP_SSC01_Config.Logic |
| V_SSP_SSC01_Config.Mode |
| V_SSP_SSC01_Config.Hysteresis % |
|
| Switching Signal Channel 2 |
| V_SSP_SSC02_Param.SP1 |
| V_SSP_SSC02_Param.SP2 |
| V_SSP_SSC02_Config.Logic |
| V_SSP_SSC02_Config.Mode |
| V_SSP_SSC02_Config.Hysteresis * 1 + 0 Hz, Dec.0 |
|
| Teach |
| V_SSP_TI_TeachSelect |
| Teach - Single Value |
V_SystemCommand, Button:=165 Description=Determine setpoint 1 in a single teach procedure. |
V_SystemCommand, Button:=166 Description=Determine setpoint 2 in a single teach procedure. |
| V_SSP_TI_TeachResult.State |
|
|
| Switching Output Setup (SO) |
| V_LED |
| V_Conf_SO1.Output Stage Mode |
| V_Conf_SO1.Source |
| V_Conf_SO1.Divider |
| V_Conf_SO1.NO/NC Operation |
If V_Conf_SO1.Timer Scale = 0:
| Timer Setup |
| V_Conf_SO1.Timer Mode |
| V_Conf_SO1.Timer Scale |
| V_Conf_SO1.Delay Duration * 1 + 0 ms, Dec.0 |
|
If V_Conf_SO1.Timer Scale = 1:
| Timer Setup |
| V_Conf_SO1.Timer Mode |
| V_Conf_SO1.Timer Scale |
| V_Conf_SO1.Delay Duration * 1 + 0 s, Dec.0 |
|
If V_Conf_SO1.Timer Scale = 2:
| Timer Setup |
| V_Conf_SO1.Timer Mode |
| V_Conf_SO1.Timer Scale |
| V_Conf_SO1.Delay Duration * 1 + 0 min, Dec.0 |
|
|
| Temperature Alarm Setup (TA) |
| V_TEMP.Maximum Temperature Warning * 1 + 0 °C, Dec.0 |
| V_TEMP.Minimum Temperature Warning * 1 + 0 °C, Dec.0 |
|
| Process Data Setup |
| V_PD_CONF.SSC1 |
| V_PD_CONF.SSC2 |
| V_PD_CONF.SO |
| V_PD_CONF.TA |
|
| Event Menu |
| V_EVENT_CONF.Activate Temperature Error Event |
| V_EVENT_CONF.Activate Over Temperature Warning Event |
| V_EVENT_CONF.Activate Under Temperature Warning Event |
|
| Parameters Menu |
| Service Functions |
V_SystemCommand, Button:=129 Description=The parameters of the technology-specific application are set to default values. Identification parameters remain unchanged. An upload to the data storage of the master will be executed, if activated in the port configuration of the master. |
V_SystemCommand, Button:=131 Description=The parameters of the device are set to factory default values and communication will be inhibited until the next power cycle. Note: Directly detach the device from the master port! |
|
| Switching Signal Channel 1 |
| V_SSP_SSC01_Param.SP1 |
| V_SSP_SSC01_Param.SP2 |
| V_SSP_SSC01_Config.Logic |
| V_SSP_SSC01_Config.Mode |
| V_SSP_SSC01_Config.Hysteresis % |
|
| Switching Signal Channel 2 |
| V_SSP_SSC02_Param.SP1 |
| V_SSP_SSC02_Param.SP2 |
| V_SSP_SSC02_Config.Logic |
| V_SSP_SSC02_Config.Mode |
| V_SSP_SSC02_Config.Hysteresis * 1 + 0 Hz, Dec.0 |
|
| Teach |
| V_SSP_TI_TeachSelect |
| Teach - Single Value |
V_SystemCommand, Button:=165 Description=Determine setpoint 1 in a single teach procedure. |
V_SystemCommand, Button:=166 Description=Determine setpoint 2 in a single teach procedure. |
| V_SSP_TI_TeachResult.State |
|
|
| Switching Output Setup (SO) |
| V_LED |
| V_Conf_SO1.Output Stage Mode |
| V_Conf_SO1.Source |
| V_Conf_SO1.Divider |
| V_Conf_SO1.NO/NC Operation |
If V_Conf_SO1.Timer Scale = 0:
| Timer Setup |
| V_Conf_SO1.Timer Mode |
| V_Conf_SO1.Timer Scale |
| V_Conf_SO1.Delay Duration * 1 + 0 ms, Dec.0 |
|
If V_Conf_SO1.Timer Scale = 1:
| Timer Setup |
| V_Conf_SO1.Timer Mode |
| V_Conf_SO1.Timer Scale |
| V_Conf_SO1.Delay Duration * 1 + 0 s, Dec.0 |
|
If V_Conf_SO1.Timer Scale = 2:
| Timer Setup |
| V_Conf_SO1.Timer Mode |
| V_Conf_SO1.Timer Scale |
| V_Conf_SO1.Delay Duration * 1 + 0 min, Dec.0 |
|
|
| Temperature Alarm Setup (TA) |
| V_TEMP.Maximum Temperature Warning * 1 + 0 °C, Dec.0 |
| V_TEMP.Minimum Temperature Warning * 1 + 0 °C, Dec.0 |
|
| Process Data Setup |
| V_PD_CONF.SSC1 |
| V_PD_CONF.SSC2 |
| V_PD_CONF.SO |
| V_PD_CONF.TA |
|
| Event Menu |
| V_EVENT_CONF.Activate Temperature Error Event |
| V_EVENT_CONF.Activate Over Temperature Warning Event |
| V_EVENT_CONF.Activate Under Temperature Warning Event |
|
Note: This page shows the content of an IODD file transformed into HTML format. In the case of disparity between this and the XML view, the content of the XML file takes precedence.
Created by IODD Viewer V1.4.