Version: V1.0Release Date: 2024-12-11


RDH 242
Vendor ID 338 (0x0152) Vendor Logo
Vendor Name Leuze electronic GmbH + Co. KG
Vendor Text Leuze electronic the sensor people
Vendor URL http://www.leuze.com
Device ID 250 (0x0000fa)
DeviceFamily RFID Reader
Features
Block Parameter yes
Data Storage yes
Profile Characteristic 0x0031 (Device Profile: Firmware Update), 0x4000 (Common Application Profile: Identification and Diagnosis)
Supported Access Locks Parameter: no, Data Storage: no, Local Parameterization: no, Local User Interface: no
Communication
IO-Link Revision V1.1
Transmission Rate230400 bit/s (COM3)
Minimum Cycle Time 2.4 ms
SIO Mode Supported no
M-Sequence CapabilityPREOPERATE = TYPE_1_V with 32 octets on-request data
OPERATE = TYPE_2_V with 32 octets on-request data
ISDU supported
Device Variant RDH 242 00
Description RFID HF-Reader, cubic
Product ID 50150662
Device Icon Device Icon
Device Symbol Device Symbol
Connection TypeM12-5 connector
Connection Symbol Connection Symbol
Connection Description M12 Connector Pin 2 not used but not isolated
- pin 1 brown; L+
- pin 2 white; Other
- pin 3 (light) blue; L-
- pin 4 black; C/Q
- pin 5 grey (slate); NC

ProcessData id=P_1

ProcessDataIn "Process Data Inputs" id=PI_1

bit length: 80
data type: 80-bit Record (subindex access not supported)

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 16 64-bit UInteger UID UID of the transponder in detection range
2 8 4-bit UInteger Transponder type Transponder type of the transponder in detection range
3 0 2-bit UInteger 0 = no signal, 1 = poor, 2 = good Transponder signal quality Transponder signal quality of the transponder in detection range
4 2 Boolean Auto RW Error Error with auto read or auto write
5 4 4-bit UInteger 0 = No transponder, 1..15 Short ID Short ID teached to the transponder in detection range
Octet 0
bit offset 79 78 77 76 75 74 73 72
subindex 1
element bit 63 62 61 60 59 58 57 56
Octet 1
bit offset 71 70 69 68 67 66 65 64
subindex 1
element bit 55 54 53 52 51 50 49 48
Octet 2
bit offset 63 62 61 60 59 58 57 56
subindex 1
element bit 47 46 45 44 43 42 41 40
Octet 3
bit offset 55 54 53 52 51 50 49 48
subindex 1
element bit 39 38 37 36 35 34 33 32
Octet 4
bit offset 47 46 45 44 43 42 41 40
subindex 1
element bit 31 30 29 28 27 26 25 24
Octet 5
bit offset 39 38 37 36 35 34 33 32
subindex 1
element bit 23 22 21 20 19 18 17 16
Octet 6
bit offset 31 30 29 28 27 26 25 24
subindex 1
element bit 15 14 13 12 11 10 9 8
Octet 7
bit offset 23 22 21 20 19 18 17 16
subindex 1
element bit 7 6 5 4 3 2 1 0
Octet 8
bit offset 15 14 13 12 11 10 9 8
subindex / / / / / / / / / / / / / / / / / / / / / / / / 2
element bit         3 2 1 0
Octet 9
bit offset 7 6 5 4 3 2 1 0
subindex 5 / / / / / / 4 3
element bit 3 2 1 0     1 0

ProcessDataOut "Process Data Outputs" id=PO_1

bit length: 8
data type: 8-bit Record (subindex access not supported)

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 0 Boolean Reader disable To enable/disable the RF field
Octet 0
bit offset 7 6 5 4 3 2 1 0
subindex / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / / 1

Standard Variable "Direct Parameters - Page 1" index=0 id=V_DirectParameters_1

description: Comprises the required parameters defining the communication characteristics and identifiers for device validation.
data type: 128-bit Record
access rights: rw

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 120 8-bit UInteger ro Reserved
2 112 8-bit UInteger ro Master Cycle Time Communication: Current communication cycle duration used by the master. This value defines the process data cycle.
3 104 8-bit UInteger ro Min Cycle Time Communication: Minimum communication cycle duration supported by the device. This value defines the lowest possible process data cycle.
4 96 8-bit UInteger ro M-Sequence Capability Communication: Information on the structure and the supported features of the communication messages.
5 88 8-bit UInteger 17 ro IO-Link Revision ID Communication: Identifier for the currently used communication protocol revision.
6 80 8-bit UInteger ro Process Data Input Length Communication: Information on width and features of the process input data (Process Data from Device to Master).
7 72 8-bit UInteger ro Process Data Output Length Communication: Information on width of the process output data (Process Data from Master to Device).
8 64 8-bit UInteger ro Vendor ID 1 Identification: Highest octet of the Vendor ID. Combined with the parameter Vendor ID 2, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community.
9 56 8-bit UInteger ro Vendor ID 2 Identification: Lowest octet of the Vendor ID. Combined with the parameter Vendor ID 1, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community.
10 48 8-bit UInteger ro Device ID 1 Identification: Highest octet of the Device ID. Combined with the parameters Device ID 2 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID.
11 40 8-bit UInteger ro Device ID 2 Identification: Middle octet of the Device ID. Combined with the parameters Device ID 1 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID.
12 32 8-bit UInteger ro Device ID 3 Identification: Lowest octet of the Device ID. Combined with the parameters Device ID 1 and 2, this parameter defines the 24-bit value of the vendor-specific Device ID.
13 24 8-bit UInteger ro Reserved
14 16 8-bit UInteger ro Reserved
15 8 8-bit UInteger ro Reserved
16 0 8-bit UInteger wo X System Command Application: Command interface for devices without ISDU support. Validity and execution of commands are not confirmed.

octet 0 1 2 3 4 5 6 7
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64
subindex 1 2 3 4 5 6 7 8
element bit 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0

octet 8 9 10 11 12 13 14 15
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
subindex 9 10 11 12 13 14 15 16
element bit 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0 7 - 0

Standard Variable "System Command" index=2 id=V_SystemCommand

description: Command interface for applications. A positive acknowledge indicates the complete and correct finalization of the requested function.
data type: 8-bit UInteger
allowed values: 80 = Start unlocking sequence, 81 = Unlocking command 1, 82 = Unlocking command 2, 128 = Device Reset, 129 = Application Reset, 130 = Restore Factory Settings, 131 = Back-to-box, 160 = Delete all Short IDs, 161 = Teach Short ID 1, 162 = Teach Short ID 2, 163 = Teach Short ID 3, 164 = Teach Short ID 4, 165 = Teach Short ID 5, 166 = Teach Short ID 6, 167 = Teach Short ID 7, 168 = Teach Short ID 8, 169 = Teach Short ID 9, 170 = Teach Short ID 10, 171 = Teach Short ID 11, 172 = Teach Short ID 12, 173 = Teach Short ID 13, 174 = Teach Short ID 14, 175 = Teach Short ID 15
access rights: wo
modifies other variables

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Standard Variable "Vendor Name" index=16 id=V_VendorName

description: The vendor name that is assigned to a Vendor ID.
data type: 64-octet String UTF-8
default value: "Leuze electronic GmbH + Co. KG"
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 8 9 10 11 12 13 14 15
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 16 17 18 19 20 21 22 23
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 24 25 26 27 28 29 30 31
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 32 33 34 35 36 37 38 39
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 40 41 42 43 44 45 46 47
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 48 49 50 51 52 53 54 55
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 56 57 58 59 60 61 62 63
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Vendor Text" index=17 id=V_VendorText

description: Additional information about the vendor.
data type: 64-octet String UTF-8
default value: "The Sensor People"
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 8 9 10 11 12 13 14 15
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 16 17 18 19 20 21 22 23
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 24 25 26 27 28 29 30 31
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 32 33 34 35 36 37 38 39
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 40 41 42 43 44 45 46 47
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 48 49 50 51 52 53 54 55
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 56 57 58 59 60 61 62 63
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Product Name" index=18 id=V_ProductName

description: Complete product name.
data type: 64-octet String UTF-8
default value: "RDH 242 00"
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 8 9 10 11 12 13 14 15
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 16 17 18 19 20 21 22 23
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 24 25 26 27 28 29 30 31
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 32 33 34 35 36 37 38 39
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 40 41 42 43 44 45 46 47
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 48 49 50 51 52 53 54 55
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 56 57 58 59 60 61 62 63
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Product ID" index=19 id=V_ProductID

description: Vendor-specific product or type identification (e.g., item number or model number).
data type: 64-octet String UTF-8
default value: "50150662"
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 8 9 10 11 12 13 14 15
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 16 17 18 19 20 21 22 23
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 24 25 26 27 28 29 30 31
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 32 33 34 35 36 37 38 39
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 40 41 42 43 44 45 46 47
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 48 49 50 51 52 53 54 55
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 56 57 58 59 60 61 62 63
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Product Text" index=20 id=V_ProductText

description: Additional product information for the device.
data type: 64-octet String UTF-8
default value: "RFID HF-Reader"
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 8 9 10 11 12 13 14 15
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 16 17 18 19 20 21 22 23
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 24 25 26 27 28 29 30 31
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 32 33 34 35 36 37 38 39
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 40 41 42 43 44 45 46 47
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 48 49 50 51 52 53 54 55
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 56 57 58 59 60 61 62 63
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Serial Number" index=21 id=V_SerialNumber

description: Unique, vendor-specific identifier of the individual device.
data type: 16-octet String UTF-8
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 8 9 10 11 12 13 14 15
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Hardware Revision" index=22 id=V_HardwareRevision

description: Unique, vendor-specific identifier of the hardware revision of the individual device.
data type: 64-octet String UTF-8
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 8 9 10 11 12 13 14 15
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 16 17 18 19 20 21 22 23
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 24 25 26 27 28 29 30 31
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 32 33 34 35 36 37 38 39
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 40 41 42 43 44 45 46 47
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 48 49 50 51 52 53 54 55
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 56 57 58 59 60 61 62 63
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Firmware Revision" index=23 id=V_FirmwareRevision

description: Unique, vendor-specific identifier of the firmware revision of the individual device.
data type: 64-octet String UTF-8
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 8 9 10 11 12 13 14 15
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 16 17 18 19 20 21 22 23
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 24 25 26 27 28 29 30 31
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 32 33 34 35 36 37 38 39
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 40 41 42 43 44 45 46 47
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 48 49 50 51 52 53 54 55
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 56 57 58 59 60 61 62 63
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Application-specific Tag" index=24 id=V_ApplicationSpecificTag

description: Possibility to mark a device with user- or application-specific information.
data type: 32-octet String UTF-8
default value: "***"
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 8 9 10 11 12 13 14 15
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 16 17 18 19 20 21 22 23
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 24 25 26 27 28 29 30 31
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Standard Variable "Error Count" index=32 id=V_ErrorCount

description: Number of errors that occurred in the technology-specific application since power on or restart.
data type: 16-bit UInteger
access rights: ro
dynamic

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Standard Variable "Device Status" index=36 id=V_DeviceStatus

description: Indicator for the current device condition and diagnosis state.
data type: 8-bit UInteger
allowed values: 0 = Device is OK, 1 = Maintenance required, 2 = Out of specification, 3 = Functional check, 4 = Failure
access rights: ro
dynamic

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Standard Variable "Detailed Device Status" index=37 id=V_DetailedDeviceStatus

description: List of all currently pending events in the device.
data type: Array[4] of 3-octet OctetString (subindex access not supported)
access rights: ro
dynamic

octet 0 1 2 3 4 5 6 7
bit offset 95 - 88 87 - 80 79 - 72 71 - 64 63 - 56 55 - 48 47 - 40 39 - 32
subindex 1 1 1 2 2 2 3 3

octet 8 9 10 11  
bit offset 31 - 24 23 - 16 15 - 8 7 - 0  
subindex 3 4 4 4  

Standard Variable "PD Input" index=40 id=V_ProcessDataInput

description: Last valid process input data of the device.
data type: see ProcessDataIn!
access rights: ro
dynamic

Standard Variable "PD Output" index=41 id=V_ProcessDataOutput

description: Last valid process output data written to the device.
data type: see ProcessDataOut!
access rights: ro
dynamic

Variable "Function Tag" index=25 id=V_CP_FunctionTag

description: Possibility to mark a device with function-specific information.
data type: 32-octet String UTF-8
default value: "***"
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 8 9 10 11 12 13 14 15
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 16 17 18 19 20 21 22 23
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 24 25 26 27 28 29 30 31
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Location Tag" index=26 id=V_CP_LocationTag

description: Possibility to mark a device with location-specific information.
data type: 32-octet String UTF-8
default value: "***"
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 8 9 10 11 12 13 14 15
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 16 17 18 19 20 21 22 23
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 24 25 26 27 28 29 30 31
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Data hold time" index=64 id=V_XRFID_DataHoldTime

description: Minimum process data hold time in ms
data type: 16-bit UInteger
allowed values: 1000..60000
default value: 1000
access rights: rw

octet 0 1  
bit offset 15 - 8 7 - 0  
element bit 15 - 8 7 - 0  

Variable "Enable transponder types" index=65 id=V_XRFID_EnableTransponderTypes

description: The device operation release for each transponder type. Multiple selection is permitted.
data type: 8-bit Record (subindex access not supported)
access rights: rw

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 0 Boolean true NXP ICODE 1 NXP ICODE 1
2 1 Boolean true ISO 15693 ISO 15693
3 2 Boolean true ISO 14443 A ISO 14443 A
4 3 Boolean true ISO 14443 B ISO 14443 B
Octet 0
bit offset 7 6 5 4 3 2 1 0
subindex / / / / / / / / / / / / / / / / / / / / / / / / 4 3 2 1

Variable "Enables AFI filter operation" index=66 id=V_XRFID_AFI_FilterOperationEnable

description: AFI (Application Family Identifier). The AFI filter is a legitimation for the ISO15693 transponder in this application: if enabled, only if the AFI on the transponder and the data stored in the AFI code are the same, the transponder can be read or written
data type: Boolean
allowed values: false = disabled, true = enabled
default value: false
access rights: rw
Octet 0
bit offset 7 6 5 4 3 2 1 0
element bit sign ext.  

Variable "AFI code" index=67 id=V_XRFID_AFI_Code

description: AFI (Application Family Identifier). The AFI filter is a legitimation for the ISO15693 transponder in this application: if enabled, only if the AFI on the transponder and the data stored in the AFI code are the same, the transponder can be read or written
data type: 8-bit UInteger
default value: 0
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Memory read or write specification" index=80 id=V_XRFID_MemoryReadWrite

description: Enable the read or write operation. Perform read or write by using the transfer buffer
data type: 24-bit Record
access rights: rw

subindex bit offset data type allowed values default value acc. restr. mod. other var. excl. from DS name description
1 8 16-bit UInteger 0..8191 0 The address of the first byte to read or write to the transponder If address and length does not with the block size of the transponder the area outside is filled with 0
2 0 8-bit UInteger 0..232 0 The number of bytes to read or write to the transponder Length in bytes which should be read or written

octet 0 1 2  
bit offset 23 - 16 15 - 8 7 - 0  
subindex 1 1 2  
element bit 15 - 8 7 - 0 7 - 0  

Variable "Memory auto read or write" index=81 id=V_XRFID_MemoryAutoReadWrite

description: Memory operation automatically after transponder is in range. If true, an auto read is performed and if false an auto write is performed.
data type: 8-bit UInteger
allowed values: 0 = Disabled, 1 = Auto write, 2 = Auto read
default value: 0
access rights: rw

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Variable "Memory read buffer" index=82 id=V_XRFID_MemoryReadBuffer

description: Reads data from the transponder with the given memory rw address and length. Unnecessary bytes are padded with 0. Bytes that do not fit are truncated.
data type: 232-octet OctetString
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 1855 - 1848 1847 - 1840 1839 - 1832 1831 - 1824 1823 - 1816 1815 - 1808 1807 - 1800 1799 - 1792

octet 8 9 10 11 12 13 14 15
bit offset 1791 - 1784 1783 - 1776 1775 - 1768 1767 - 1760 1759 - 1752 1751 - 1744 1743 - 1736 1735 - 1728

octet 16 17 18 19 20 21 22 23
bit offset 1727 - 1720 1719 - 1712 1711 - 1704 1703 - 1696 1695 - 1688 1687 - 1680 1679 - 1672 1671 - 1664

octet 24 25 26 27 28 29 30 31
bit offset 1663 - 1656 1655 - 1648 1647 - 1640 1639 - 1632 1631 - 1624 1623 - 1616 1615 - 1608 1607 - 1600

octet 32 33 34 35 36 37 38 39
bit offset 1599 - 1592 1591 - 1584 1583 - 1576 1575 - 1568 1567 - 1560 1559 - 1552 1551 - 1544 1543 - 1536

octet 40 41 42 43 44 45 46 47
bit offset 1535 - 1528 1527 - 1520 1519 - 1512 1511 - 1504 1503 - 1496 1495 - 1488 1487 - 1480 1479 - 1472

octet 48 49 50 51 52 53 54 55
bit offset 1471 - 1464 1463 - 1456 1455 - 1448 1447 - 1440 1439 - 1432 1431 - 1424 1423 - 1416 1415 - 1408

octet 56 57 58 59 60 61 62 63
bit offset 1407 - 1400 1399 - 1392 1391 - 1384 1383 - 1376 1375 - 1368 1367 - 1360 1359 - 1352 1351 - 1344

octet 64 65 66 67 68 69 70 71
bit offset 1343 - 1336 1335 - 1328 1327 - 1320 1319 - 1312 1311 - 1304 1303 - 1296 1295 - 1288 1287 - 1280

octet 72 73 74 75 76 77 78 79
bit offset 1279 - 1272 1271 - 1264 1263 - 1256 1255 - 1248 1247 - 1240 1239 - 1232 1231 - 1224 1223 - 1216

octet 80 81 82 83 84 85 86 87
bit offset 1215 - 1208 1207 - 1200 1199 - 1192 1191 - 1184 1183 - 1176 1175 - 1168 1167 - 1160 1159 - 1152

octet 88 89 90 91 92 93 94 95
bit offset 1151 - 1144 1143 - 1136 1135 - 1128 1127 - 1120 1119 - 1112 1111 - 1104 1103 - 1096 1095 - 1088

octet 96 97 98 99 100 101 102 103
bit offset 1087 - 1080 1079 - 1072 1071 - 1064 1063 - 1056 1055 - 1048 1047 - 1040 1039 - 1032 1031 - 1024

octet 104 105 106 107 108 109 110 111
bit offset 1023 - 1016 1015 - 1008 1007 - 1000 999 - 992 991 - 984 983 - 976 975 - 968 967 - 960

octet 112 113 114 115 116 117 118 119
bit offset 959 - 952 951 - 944 943 - 936 935 - 928 927 - 920 919 - 912 911 - 904 903 - 896

octet 120 121 122 123 124 125 126 127
bit offset 895 - 888 887 - 880 879 - 872 871 - 864 863 - 856 855 - 848 847 - 840 839 - 832

octet 128 129 130 131 132 133 134 135
bit offset 831 - 824 823 - 816 815 - 808 807 - 800 799 - 792 791 - 784 783 - 776 775 - 768

octet 136 137 138 139 140 141 142 143
bit offset 767 - 760 759 - 752 751 - 744 743 - 736 735 - 728 727 - 720 719 - 712 711 - 704

octet 144 145 146 147 148 149 150 151
bit offset 703 - 696 695 - 688 687 - 680 679 - 672 671 - 664 663 - 656 655 - 648 647 - 640

octet 152 153 154 155 156 157 158 159
bit offset 639 - 632 631 - 624 623 - 616 615 - 608 607 - 600 599 - 592 591 - 584 583 - 576

octet 160 161 162 163 164 165 166 167
bit offset 575 - 568 567 - 560 559 - 552 551 - 544 543 - 536 535 - 528 527 - 520 519 - 512

octet 168 169 170 171 172 173 174 175
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 176 177 178 179 180 181 182 183
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 184 185 186 187 188 189 190 191
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 192 193 194 195 196 197 198 199
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 200 201 202 203 204 205 206 207
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 208 209 210 211 212 213 214 215
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 216 217 218 219 220 221 222 223
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 224 225 226 227 228 229 230 231
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Memory write buffer" index=83 id=V_XRFID_MemoryWriteBuffer

description: Writes data to the transponder with the given memory rw address and length. Unnecessary bytes are not written. If the variable contains fewer bytes than addressed, then the missing bytes are filled with 0.
data type: 232-octet OctetString
access rights: wo

octet 0 1 2 3 4 5 6 7
bit offset 1855 - 1848 1847 - 1840 1839 - 1832 1831 - 1824 1823 - 1816 1815 - 1808 1807 - 1800 1799 - 1792

octet 8 9 10 11 12 13 14 15
bit offset 1791 - 1784 1783 - 1776 1775 - 1768 1767 - 1760 1759 - 1752 1751 - 1744 1743 - 1736 1735 - 1728

octet 16 17 18 19 20 21 22 23
bit offset 1727 - 1720 1719 - 1712 1711 - 1704 1703 - 1696 1695 - 1688 1687 - 1680 1679 - 1672 1671 - 1664

octet 24 25 26 27 28 29 30 31
bit offset 1663 - 1656 1655 - 1648 1647 - 1640 1639 - 1632 1631 - 1624 1623 - 1616 1615 - 1608 1607 - 1600

octet 32 33 34 35 36 37 38 39
bit offset 1599 - 1592 1591 - 1584 1583 - 1576 1575 - 1568 1567 - 1560 1559 - 1552 1551 - 1544 1543 - 1536

octet 40 41 42 43 44 45 46 47
bit offset 1535 - 1528 1527 - 1520 1519 - 1512 1511 - 1504 1503 - 1496 1495 - 1488 1487 - 1480 1479 - 1472

octet 48 49 50 51 52 53 54 55
bit offset 1471 - 1464 1463 - 1456 1455 - 1448 1447 - 1440 1439 - 1432 1431 - 1424 1423 - 1416 1415 - 1408

octet 56 57 58 59 60 61 62 63
bit offset 1407 - 1400 1399 - 1392 1391 - 1384 1383 - 1376 1375 - 1368 1367 - 1360 1359 - 1352 1351 - 1344

octet 64 65 66 67 68 69 70 71
bit offset 1343 - 1336 1335 - 1328 1327 - 1320 1319 - 1312 1311 - 1304 1303 - 1296 1295 - 1288 1287 - 1280

octet 72 73 74 75 76 77 78 79
bit offset 1279 - 1272 1271 - 1264 1263 - 1256 1255 - 1248 1247 - 1240 1239 - 1232 1231 - 1224 1223 - 1216

octet 80 81 82 83 84 85 86 87
bit offset 1215 - 1208 1207 - 1200 1199 - 1192 1191 - 1184 1183 - 1176 1175 - 1168 1167 - 1160 1159 - 1152

octet 88 89 90 91 92 93 94 95
bit offset 1151 - 1144 1143 - 1136 1135 - 1128 1127 - 1120 1119 - 1112 1111 - 1104 1103 - 1096 1095 - 1088

octet 96 97 98 99 100 101 102 103
bit offset 1087 - 1080 1079 - 1072 1071 - 1064 1063 - 1056 1055 - 1048 1047 - 1040 1039 - 1032 1031 - 1024

octet 104 105 106 107 108 109 110 111
bit offset 1023 - 1016 1015 - 1008 1007 - 1000 999 - 992 991 - 984 983 - 976 975 - 968 967 - 960

octet 112 113 114 115 116 117 118 119
bit offset 959 - 952 951 - 944 943 - 936 935 - 928 927 - 920 919 - 912 911 - 904 903 - 896

octet 120 121 122 123 124 125 126 127
bit offset 895 - 888 887 - 880 879 - 872 871 - 864 863 - 856 855 - 848 847 - 840 839 - 832

octet 128 129 130 131 132 133 134 135
bit offset 831 - 824 823 - 816 815 - 808 807 - 800 799 - 792 791 - 784 783 - 776 775 - 768

octet 136 137 138 139 140 141 142 143
bit offset 767 - 760 759 - 752 751 - 744 743 - 736 735 - 728 727 - 720 719 - 712 711 - 704

octet 144 145 146 147 148 149 150 151
bit offset 703 - 696 695 - 688 687 - 680 679 - 672 671 - 664 663 - 656 655 - 648 647 - 640

octet 152 153 154 155 156 157 158 159
bit offset 639 - 632 631 - 624 623 - 616 615 - 608 607 - 600 599 - 592 591 - 584 583 - 576

octet 160 161 162 163 164 165 166 167
bit offset 575 - 568 567 - 560 559 - 552 551 - 544 543 - 536 535 - 528 527 - 520 519 - 512

octet 168 169 170 171 172 173 174 175
bit offset 511 - 504 503 - 496 495 - 488 487 - 480 479 - 472 471 - 464 463 - 456 455 - 448

octet 176 177 178 179 180 181 182 183
bit offset 447 - 440 439 - 432 431 - 424 423 - 416 415 - 408 407 - 400 399 - 392 391 - 384

octet 184 185 186 187 188 189 190 191
bit offset 383 - 376 375 - 368 367 - 360 359 - 352 351 - 344 343 - 336 335 - 328 327 - 320

octet 192 193 194 195 196 197 198 199
bit offset 319 - 312 311 - 304 303 - 296 295 - 288 287 - 280 279 - 272 271 - 264 263 - 256

octet 200 201 202 203 204 205 206 207
bit offset 255 - 248 247 - 240 239 - 232 231 - 224 223 - 216 215 - 208 207 - 200 199 - 192

octet 208 209 210 211 212 213 214 215
bit offset 191 - 184 183 - 176 175 - 168 167 - 160 159 - 152 151 - 144 143 - 136 135 - 128

octet 216 217 218 219 220 221 222 223
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 224 225 226 227 228 229 230 231
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 1 teach value" index=100 id=V_XRFID_TeachValueShortUID1

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 2 teach value" index=101 id=V_XRFID_TeachValueShortUID2

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 3 teach value" index=102 id=V_XRFID_TeachValueShortUID3

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 4 teach value" index=103 id=V_XRFID_TeachValueShortUID4

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 5 teach value" index=104 id=V_XRFID_TeachValueShortUID5

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 6 teach value" index=105 id=V_XRFID_TeachValueShortUID6

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 7 teach value" index=106 id=V_XRFID_TeachValueShortUID7

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 8 teach value" index=107 id=V_XRFID_TeachValueShortUID8

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 9 teach value" index=108 id=V_XRFID_TeachValueShortUID9

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 10 teach value" index=109 id=V_XRFID_TeachValueShortUID10

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 11 teach value" index=110 id=V_XRFID_TeachValueShortUID11

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 12 teach value" index=111 id=V_XRFID_TeachValueShortUID12

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 13 teach value" index=112 id=V_XRFID_TeachValueShortUID13

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 14 teach value" index=113 id=V_XRFID_TeachValueShortUID14

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Short ID 15 teach value" index=114 id=V_XRFID_TeachValueShortUID15

description: If a UID has been taught into the storage space of a Short UID, then the Short ID is displayed in the process data when the associated UID has been recognized.
data type: 64-bit UInteger
allowed values: 0 = not set, 1..4294967295
default value: 0
access rights: rw

octet 0 1 2 3 4 5 6 7
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0
element bit 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Operating Hours" index=190 id=V_X_OperatingHours

data type: 32-bit Integer
default value: 0
access rights: ro
dynamic

octet 0 1 2 3  
bit offset 31 - 24 23 - 16 15 - 8 7 - 0  
element bit 31 - 24 23 - 16 15 - 8 7 - 0  

Variable "Hardware Identification Key" index=17342 id=V_FU_HW_ID_Key

description: Identifies the hardware for compatibility check with the firmware to be installed.
data type: 16-octet String UTF-8
default value: "RDH 242"
access rights: ro

octet 0 1 2 3 4 5 6 7
bit offset 127 - 120 119 - 112 111 - 104 103 - 96 95 - 88 87 - 80 79 - 72 71 - 64

octet 8 9 10 11 12 13 14 15
bit offset 63 - 56 55 - 48 47 - 40 39 - 32 31 - 24 23 - 16 15 - 8 7 - 0

Variable "Bootmode Status" index=17343 id=V_FU_BootmodeStatus

data type: 8-bit UInteger
allowed values: 0 = Bootloader is inactive, 1 = Bootloader is active
access rights: ro
dynamic

octet 0  
bit offset 7 - 0  
element bit 7 - 0  

Events

CodeTypeNameDescription
6200 (0x1838)ErrorEvent 1
6201 (0x1839)ErrorEvent 2

Process Data Formatting

Formatting for Process Data id=PI_1
Subindex 1: Hex
Subindex 2:
Subindex 3:
Subindex 4:
Subindex 5:

Formatting for Process Data id=PO_1
Subindex 1:

Operator Menus

Identification Menu
V_VendorName
V_VendorText
V_ProductName
V_ProductText
V_ProductID
V_SerialNumber
V_HardwareRevision
V_FirmwareRevision
V_FU_HW_ID_Key
V_CP_FunctionTag, ro
V_CP_LocationTag, ro
V_ApplicationSpecificTag, ro

Parameters Menu
Device Parameterization
V_XRFID_DataHoldTime ms, ro
V_XRFID_EnableTransponderTypes, ro
V_XRFID_AFI_FilterOperationEnable, ro
V_XRFID_AFI_Code, ro
Memory Operation
V_XRFID_MemoryReadWrite
V_XRFID_MemoryAutoReadWrite, ro
V_XRFID_MemoryReadBuffer, Hex
Teaching Short IDs
V_XRFID_TeachValueShortUID1, ro Hex
V_XRFID_TeachValueShortUID2, ro Hex
V_XRFID_TeachValueShortUID3, ro Hex
V_XRFID_TeachValueShortUID4, ro Hex
V_XRFID_TeachValueShortUID5, ro Hex
V_XRFID_TeachValueShortUID6, ro Hex
V_XRFID_TeachValueShortUID7, ro Hex
V_XRFID_TeachValueShortUID8, ro Hex
V_XRFID_TeachValueShortUID9, ro Hex
V_XRFID_TeachValueShortUID10, ro Hex
V_XRFID_TeachValueShortUID11, ro Hex
V_XRFID_TeachValueShortUID12, ro Hex
V_XRFID_TeachValueShortUID13, ro Hex
V_XRFID_TeachValueShortUID14, ro Hex
V_XRFID_TeachValueShortUID15, ro Hex

Observation Menu
Process Data Inputs
V_ProcessDataInput
Process Data Outputs
V_ProcessDataOutput

Diagnosis Menu
Device Status Information
V_DeviceStatus
V_DetailedDeviceStatus
V_ErrorCount
Device Diagnosis
V_X_OperatingHours * 0.01 h, Dec.2

Maintenance Menus

Identification Menu
V_VendorName
V_VendorText
V_ProductName
V_ProductText
V_ProductID
V_SerialNumber
V_HardwareRevision
V_FirmwareRevision
V_FU_HW_ID_Key
V_CP_FunctionTag
V_CP_LocationTag
V_ApplicationSpecificTag

Parameters Menu
Device Parameterization
V_XRFID_DataHoldTime ms
V_XRFID_EnableTransponderTypes
V_XRFID_AFI_FilterOperationEnable
V_XRFID_AFI_Code
Memory Operation
V_XRFID_MemoryReadWrite
V_XRFID_MemoryAutoReadWrite
V_XRFID_MemoryReadBuffer, Hex
V_XRFID_MemoryWriteBuffer, Hex
Teaching Short IDs
V_SystemCommand, Button:=160
Description=Deletes all Short IDs
V_SystemCommand, Button:=161
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID1, Hex
V_SystemCommand, Button:=162
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID2, Hex
V_SystemCommand, Button:=163
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID3, Hex
V_SystemCommand, Button:=164
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID4, Hex
V_SystemCommand, Button:=165
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID5, Hex
V_SystemCommand, Button:=166
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID6, Hex
V_SystemCommand, Button:=167
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID7, Hex
V_SystemCommand, Button:=168
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID8, Hex
V_SystemCommand, Button:=169
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID9, Hex
V_SystemCommand, Button:=170
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID10, Hex
V_SystemCommand, Button:=171
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID11, Hex
V_SystemCommand, Button:=172
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID12, Hex
V_SystemCommand, Button:=173
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID13, Hex
V_SystemCommand, Button:=174
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID14, Hex
V_SystemCommand, Button:=175
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID15, Hex
General Settings
V_SystemCommand, Button:=128
Description=A warm start is triggered and the device will be set to an initial state. The communication will be interrupted by the device and then reinitiated by the master.
V_SystemCommand, Button:=129
Description=The parameter of the technology-specific application are set to default values. Identification parameter remain unchanged. An upload to the data storage of the master will be executed, if activated in the port configuration of the master.
V_SystemCommand, Button:=130
Description=The parameter of the device are reset to factory settings. Note: A download of the data storage may be executed on the next power cycle and overwrite the factory default settings!
V_SystemCommand, Button:=131
Description=The parameter of the device are set to factory default values and communication will be inhibited until the next power cycle. Note: Directly detach the device from the master port!

Observation Menu
Process Data Inputs
V_ProcessDataInput
Process Data Outputs
V_ProcessDataOutput

Diagnosis Menu
Device Status Information
V_DeviceStatus
V_DetailedDeviceStatus
V_ErrorCount
Device Diagnosis
V_X_OperatingHours * 0.01 h, Dec.2
Service Functions
V_SystemCommand, Button:=131
Description=The parameter of the device are set to factory default values and communication will be inhibited until the next power cycle. Note: Directly detach the device from the master port!
V_SystemCommand, Button:=128
Description=A warm start is triggered and the device will be set to an initial state. The communication will be interrupted by the device and then reinitiated by the master.

Commissioning Menus

Identification Menu
V_VendorName
V_VendorText
V_ProductName
V_ProductText
V_ProductID
V_SerialNumber
V_HardwareRevision
V_FirmwareRevision
V_FU_HW_ID_Key
V_CP_FunctionTag
V_CP_LocationTag
V_ApplicationSpecificTag

Parameters Menu
Device Parameterization
V_XRFID_DataHoldTime ms
V_XRFID_EnableTransponderTypes
V_XRFID_AFI_FilterOperationEnable
V_XRFID_AFI_Code
Memory Operation
V_XRFID_MemoryReadWrite
V_XRFID_MemoryAutoReadWrite
V_XRFID_MemoryReadBuffer, Hex
V_XRFID_MemoryWriteBuffer, Hex
Teaching Short IDs
V_SystemCommand, Button:=160
Description=Deletes all Short IDs
V_SystemCommand, Button:=161
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID1, Hex
V_SystemCommand, Button:=162
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID2, Hex
V_SystemCommand, Button:=163
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID3, Hex
V_SystemCommand, Button:=164
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID4, Hex
V_SystemCommand, Button:=165
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID5, Hex
V_SystemCommand, Button:=166
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID6, Hex
V_SystemCommand, Button:=167
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID7, Hex
V_SystemCommand, Button:=168
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID8, Hex
V_SystemCommand, Button:=169
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID9, Hex
V_SystemCommand, Button:=170
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID10, Hex
V_SystemCommand, Button:=171
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID11, Hex
V_SystemCommand, Button:=172
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID12, Hex
V_SystemCommand, Button:=173
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID13, Hex
V_SystemCommand, Button:=174
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID14, Hex
V_SystemCommand, Button:=175
Description=Writes the UID of the currently read transponder into the corresponding memory location
V_XRFID_TeachValueShortUID15, Hex
General Settings
V_SystemCommand, Button:=128
Description=A warm start is triggered and the device will be set to an initial state. The communication will be interrupted by the device and then reinitiated by the master.
V_SystemCommand, Button:=129
Description=The parameter of the technology-specific application are set to default values. Identification parameter remain unchanged. An upload to the data storage of the master will be executed, if activated in the port configuration of the master.
V_SystemCommand, Button:=130
Description=The parameter of the device are reset to factory settings. Note: A download of the data storage may be executed on the next power cycle and overwrite the factory default settings!
V_SystemCommand, Button:=131
Description=The parameter of the device are set to factory default values and communication will be inhibited until the next power cycle. Note: Directly detach the device from the master port!

Observation Menu
Process Data Inputs
V_ProcessDataInput
Process Data Outputs
V_ProcessDataOutput

Diagnosis Menu
Device Status Information
V_DeviceStatus
V_DetailedDeviceStatus
V_ErrorCount
Device Diagnosis
V_X_OperatingHours * 0.01 h, Dec.2
Service Functions
V_SystemCommand, Button:=131
Description=The parameter of the device are set to factory default values and communication will be inhibited until the next power cycle. Note: Directly detach the device from the master port!
V_SystemCommand, Button:=128
Description=A warm start is triggered and the device will be set to an initial state. The communication will be interrupted by the device and then reinitiated by the master.

Note: This page shows the content of an IODD file transformed into HTML format. In the case of disparity between this and the XML view, the content of the XML file takes precedence.
Created by IODD Viewer V1.4.