subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
1 |
120 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
2 |
112 |
8-bit UInteger |
|
0 |
ro |
|
|
Master Cycle Time |
Communication: Current communication cycle duration used by the master. This value defines the process data cycle. |
3 |
104 |
8-bit UInteger |
|
23 |
ro |
|
|
Min Cycle Time |
Communication: Minimum communication cycle duration supported by the device. This value defines the lowest possible process data cycle. |
4 |
96 |
8-bit UInteger |
|
0 |
ro |
|
|
M-Sequence Capability |
Communication: Information on the structure and the supported features of the communication messages. |
5 |
88 |
8-bit UInteger |
|
17 |
ro |
|
|
IO-Link Revision ID |
Communication: Identifier for the currently used communication protocol revision. |
6 |
80 |
8-bit UInteger |
|
72 |
ro |
|
|
Process Data Input Length |
Communication: Information on width and features of the process input data (Process Data from Device to Master). |
7 |
72 |
8-bit UInteger |
|
1 |
ro |
|
|
Process Data Output Length |
Communication: Information on width of the process output data (Process Data from Master to Device). |
8 |
64 |
8-bit UInteger |
|
1 |
ro |
|
|
Vendor ID 1 |
Identification: Highest octet of the Vendor ID. Combined with the parameter Vendor ID 2, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community. |
9 |
56 |
8-bit UInteger |
|
82 |
ro |
|
|
Vendor ID 2 |
Identification: Lowest octet of the Vendor ID. Combined with the parameter Vendor ID 1, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community. |
10 |
48 |
8-bit UInteger |
|
0 |
ro |
|
|
Device ID 1 |
Identification: Highest octet of the Device ID. Combined with the parameters Device ID 2 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID. |
11 |
40 |
8-bit UInteger |
|
8 |
ro |
|
|
Device ID 2 |
Identification: Middle octet of the Device ID. Combined with the parameters Device ID 1 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID. |
12 |
32 |
8-bit UInteger |
|
63 |
ro |
|
|
Device ID 3 |
Identification: Lowest octet of the Device ID. Combined with the parameters Device ID 1 and 2, this parameter defines the 24-bit value of the vendor-specific Device ID. |
13 |
24 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
14 |
16 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
15 |
8 |
8-bit UInteger |
|
|
ro |
|
|
Reserved |
|
16 |
0 |
8-bit UInteger |
160 = Error Confirmation, 161 = Teach 11% (Standard Sensitivity), 162 = Teach 30% (Decreased Sensitivity), 163 = dark switching, 164 = light switching, 170 = Enable Configuration Mode, 171 = Reload last Teach (WORKING), 172 = Restore factory defaults, 173 = Save current parameters to device, 174 = Enable Sensor Mode, 191 = Enable ADC Signal Process Data Output |
|
wo |
X |
|
System Command |
Application: Command interface for devices without ISDU support. Validity and execution of commands are not confirmed. |
subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
1 |
120 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 1 |
|
2 |
112 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 2 |
|
3 |
104 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 3 |
|
4 |
96 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 4 |
|
5 |
88 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 5 |
|
6 |
80 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 6 |
|
7 |
72 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 7 |
|
8 |
64 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 8 |
|
9 |
56 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 9 |
|
10 |
48 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 10 |
|
11 |
40 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 11 |
|
12 |
32 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 12 |
|
13 |
24 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 13 |
|
14 |
16 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 14 |
|
15 |
8 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 15 |
|
16 |
0 |
8-bit UInteger |
|
|
|
|
|
Device-specific Parameter 16 |
|
subindex |
bit offset |
data type |
allowed values |
default value |
acc. restr. |
mod. other var. |
excl. from DS |
name |
description |
2 |
104 |
8-bit UInteger |
|
|
|
|
|
Off Limit |
Off Limit |
3 |
96 |
8-bit UInteger |
|
|
|
|
|
On Limit |
On Limit |
6 |
77 |
Boolean |
false = Disabled, true = Enabled |
0 |
|
|
|
Key Lock |
Key Lock; IO-Link Parameter overrides IN2 Input/PD |
8 |
74 |
2-bit UInteger |
0 = Inverted Switching Output, 1 = Switching Output, 2 = Warning Output |
0 |
|
|
|
Q2 logic function |
|
10 |
70 |
2-bit UInteger |
0 = On delay, 1 = Off delay, 2 = pulse stretching, 3 = pulse suppression |
1 |
|
|
|
Delay Function (internal delay unit) |
Operating mode of the internal delay unit |
11 |
68 |
2-bit UInteger |
0 = 1ms, 1 = 10ms, 2 = 100ms, 3 = 1000ms |
3 |
|
|
|
Time base (internal delay unit) |
1ms, 10ms, 100ms, 1000ms |
12 |
64 |
4-bit UInteger |
|
5 |
|
|
|
Multiplication factor for time base (internal delay unit) |
1-15 |
18 |
58 |
Boolean |
false = light switching, true = dark switching |
0 |
|
|
|
Light/Dark Switching |
Light/Dark Switching: adjusting the switching behavior of the switching output |
20 |
56 |
Boolean |
false = Disabled, true = Enabled |
0 |
|
|
|
Internal Delay Unit (based on object) |
Enable Internal Delay Unit |
26 |
8 |
8-bit UInteger |
0 = Switching Signal and Status, 1 = Analog ADC value and Switching Signal |
0 |
ro |
|
|
PDI Content |
|
32 |
127 |
Boolean |
false = finished, true = running |
0 |
ro |
|
|
Status Teach/Command |
Value is re-read after new command. All status bits are valid after finished command. |
33 |
126 |
Boolean |
false = no, true = yes |
0 |
ro |
|
|
Command accepted |
|
36 |
123 |
Boolean |
false = no, true = yes |
0 |
ro |
|
|
Teach Error |
|
37 |
122 |
Boolean |
false = no, true = yes |
0 |
ro |
|
|
Last values restored |
|
38 |
121 |
Boolean |
false = no, true = yes |
0 |
ro |
|
|
Reception level too high |
|
39 |
120 |
Boolean |
false = no, true = yes |
0 |
ro |
|
|
Reception level too low |
|
Parameters Menu |
Commands |
V_DirectParameters_1.System Command, wo Button:=161 |
V_DirectParameters_1.System Command, wo Button:=162 |
V_DirectParameters_1.System Command, wo Button:=163 |
V_DirectParameters_1.System Command, wo Button:=164 |
V_DirectParameters_1.System Command, wo Button:=170 |
V_DirectParameters_1.System Command, wo Button:=171 |
V_DirectParameters_1.System Command, wo Button:=172 |
V_DirectParameters_1.System Command, wo Button:=173 |
V_DirectParameters_1.System Command, wo Button:=174 Description=Enable Sensor Mode |
V_DirectParameters_1.System Command, wo Button:=191 |
|
Status |
V_DirectParameters.Status Teach/Command |
V_DirectParameters.Command accepted |
V_DirectParameters.Teach Error |
V_DirectParameters.Last values restored |
V_DirectParameters.Reception level too high |
V_DirectParameters.Reception level too low |
V_DirectParameters.PDI Content |
|
In2 / Out2 function |
V_DirectParameters.Key Lock |
V_DirectParameters.Q2 logic function |
|
Parameter |
V_DirectParameters.Light/Dark Switching |
V_DirectParameters.Internal Delay Unit (based on object) |
|
Delay Unit |
V_DirectParameters.Delay Function (internal delay unit) |
V_DirectParameters.Time base (internal delay unit) |
V_DirectParameters.Multiplication factor for time base (internal delay unit) |
|
Parameters Menu |
Commands |
V_DirectParameters_1.System Command, wo Button:=161 |
V_DirectParameters_1.System Command, wo Button:=162 |
V_DirectParameters_1.System Command, wo Button:=163 |
V_DirectParameters_1.System Command, wo Button:=164 |
V_DirectParameters_1.System Command, wo Button:=170 |
V_DirectParameters_1.System Command, wo Button:=171 |
V_DirectParameters_1.System Command, wo Button:=172 |
V_DirectParameters_1.System Command, wo Button:=173 |
V_DirectParameters_1.System Command, wo Button:=174 Description=Enable Sensor Mode |
V_DirectParameters_1.System Command, wo Button:=191 |
|
Status |
V_DirectParameters.Status Teach/Command |
V_DirectParameters.Command accepted |
V_DirectParameters.Teach Error |
V_DirectParameters.Last values restored |
V_DirectParameters.Reception level too high |
V_DirectParameters.Reception level too low |
V_DirectParameters.PDI Content |
|
In2 / Out2 function |
V_DirectParameters.Key Lock |
V_DirectParameters.Q2 logic function |
|
Parameter |
V_DirectParameters.Light/Dark Switching |
V_DirectParameters.Internal Delay Unit (based on object) |
|
Delay Unit |
V_DirectParameters.Delay Function (internal delay unit) |
V_DirectParameters.Time base (internal delay unit) |
V_DirectParameters.Multiplication factor for time base (internal delay unit) |
|
Parameters Menu |
Commands |
V_DirectParameters_1.System Command, wo Button:=161 |
V_DirectParameters_1.System Command, wo Button:=162 |
V_DirectParameters_1.System Command, wo Button:=163 |
V_DirectParameters_1.System Command, wo Button:=164 |
V_DirectParameters_1.System Command, wo Button:=170 |
V_DirectParameters_1.System Command, wo Button:=171 |
V_DirectParameters_1.System Command, wo Button:=172 |
V_DirectParameters_1.System Command, wo Button:=173 |
V_DirectParameters_1.System Command, wo Button:=174 Description=Enable Sensor Mode |
V_DirectParameters_1.System Command, wo Button:=191 |
|
Status |
V_DirectParameters.Status Teach/Command |
V_DirectParameters.Command accepted |
V_DirectParameters.Teach Error |
V_DirectParameters.Last values restored |
V_DirectParameters.Reception level too high |
V_DirectParameters.Reception level too low |
V_DirectParameters.PDI Content |
|
In2 / Out2 function |
V_DirectParameters.Key Lock |
V_DirectParameters.Q2 logic function |
|
Parameter |
V_DirectParameters.Light/Dark Switching |
V_DirectParameters.Internal Delay Unit (based on object) |
|
Delay Unit |
V_DirectParameters.Delay Function (internal delay unit) |
V_DirectParameters.Time base (internal delay unit) |
V_DirectParameters.Multiplication factor for time base (internal delay unit) |
|
Note: This page shows the content of an IODD file transformed into HTML format. In the case of disparity between this and the XML view, the content of the XML file takes precedence.
Created by IODD Viewer V1.4.