Version: V1.2 | Release Date: 2024-01-31 |
DMU420B-500.3/LC-M8 | ||
---|---|---|
Vendor ID | 338 (0x0152) | ![]() |
Vendor Name | Leuze electronic GmbH + Co. KG | |
Vendor Text | The Sensor People | |
Vendor URL | www.leuze.com | |
Device ID | 3099 (0x000c1b) | |
DeviceFamily | DMU… series | |
Features | ||
Block Parameter | yes | |
Data Storage | yes | |
Profile Characteristic | 0x0001 (Device Profile: Generic Profiled Sensor), 0x000d (Device Profile: Measuring Sensor, high resolution, sensor control function), 0x4000 (Common Application Profile: Identification and Diagnosis), 0x8001 (Function Class: Multiple switching signal), 0x8004 (Function Class: Teach channel) | |
Supported Access Locks | Parameter: no, Data Storage: yes, Local Parameterization: no, Local User Interface: no | |
Communication | ||
IO-Link Revision | V1.1 | |
Transmission Rate | 38400 bit/s (COM2) | |
Minimum Cycle Time | 8 ms | |
SIO Mode Supported | yes | |
M-Sequence Capability | PREOPERATE = TYPE_1_V with 8 octets on-request data OPERATE = TYPE_2_V with 8 octets on-request data ISDU supported | |
Device Variant | DMU420B-500.3/LC-M8 | |
Description | Ultrasonic Distance Sensor | |
Product ID | 50150579 | |
Device Icon | ![]() | |
Device Symbol | ![]() | |
Connection Type | M8 connector | |
Connection Symbol | ![]() | |
- pin 1 | brown; L+ | |
- pin 2 | white; Other; Analog Out | |
- pin 3 | (light) blue; L- | |
- pin 4 | black; C/Q |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 16 | 32-bit Integer | Measurement Value | ||||||
2 | 8 | 8-bit Integer | Scale | ||||||
3 | 7 | Boolean | Not used | ||||||
5 | 5 | Boolean | SSC.4/Counter | ||||||
7 | 3 | Boolean | Alarm Output | ||||||
8 | 2 | Boolean | Quality Bit | ||||||
9 | 1 | Boolean | SSC.2/Distance | ||||||
10 | 0 | Boolean | SSC.1/Distance |
bit offset | 47 | 46 | 45 | 44 | 43 | 42 | 41 | 40 |
subindex | 1 | |||||||
element bit | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
bit offset | 39 | 38 | 37 | 36 | 35 | 34 | 33 | 32 |
subindex | 1 | |||||||
element bit | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
bit offset | 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
subindex | 1 | |||||||
element bit | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
bit offset | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
subindex | 1 | |||||||
element bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
bit offset | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
subindex | 2 | |||||||
element bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
bit offset | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
subindex | 3 | / / / / / / | 5 | / / / / / / | 7 | 8 | 9 | 10 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 2 | Boolean | Trigger | ||||||
2 | 1 | Boolean | Find Me | ||||||
3 | 0 | Boolean | Disable Transducer |
bit offset | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
subindex | 1 | 2 | 3 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 120 | 8-bit UInteger | ro | Reserved | |||||
2 | 112 | 8-bit UInteger | ro | Master Cycle Time | Communication: Current communication cycle duration used by the master. This value defines the process data cycle. | ||||
3 | 104 | 8-bit UInteger | ro | Min Cycle Time | Communication: Minimum communication cycle duration supported by the device. This value defines the lowest possible process data cycle. | ||||
4 | 96 | 8-bit UInteger | ro | M-Sequence Capability | Communication: Information on the structure and the supported features of the communication messages. | ||||
5 | 88 | 8-bit UInteger | 17 | ro | IO-Link Revision ID | Communication: Identifier for the currently used communication protocol revision. | |||
6 | 80 | 8-bit UInteger | ro | Process Data Input Length | Communication: Information on width and features of the process input data (Process Data from Device to Master). | ||||
7 | 72 | 8-bit UInteger | ro | Process Data Output Length | Communication: Information on width of the process output data (Process Data from Master to Device). | ||||
8 | 64 | 8-bit UInteger | ro | Vendor ID 1 | Identification: Highest octet of the Vendor ID. Combined with the parameter Vendor ID 2, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community. | ||||
9 | 56 | 8-bit UInteger | ro | Vendor ID 2 | Identification: Lowest octet of the Vendor ID. Combined with the parameter Vendor ID 1, this parameter defines the 16-bit value of the unique Vendor ID as assigned by the IO-Link Community. | ||||
10 | 48 | 8-bit UInteger | ro | Device ID 1 | Identification: Highest octet of the Device ID. Combined with the parameters Device ID 2 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID. | ||||
11 | 40 | 8-bit UInteger | ro | Device ID 2 | Identification: Middle octet of the Device ID. Combined with the parameters Device ID 1 and 3, this parameter defines the 24-bit value of the vendor-specific Device ID. | ||||
12 | 32 | 8-bit UInteger | ro | Device ID 3 | Identification: Lowest octet of the Device ID. Combined with the parameters Device ID 1 and 2, this parameter defines the 24-bit value of the vendor-specific Device ID. | ||||
13 | 24 | 8-bit UInteger | ro | Reserved | |||||
14 | 16 | 8-bit UInteger | ro | Reserved | |||||
15 | 8 | 8-bit UInteger | ro | Reserved | |||||
16 | 0 | 8-bit UInteger | wo | X | System Command | Application: Command interface for devices without ISDU support. Validity and execution of commands are not confirmed. |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
subindex | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 |
element bit | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 9 | 10 | 11 | 12 | 13 | 14 | 15 | 16 |
element bit | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 120 | 8-bit UInteger | Device-specific Parameter 1 | ||||||
2 | 112 | 8-bit UInteger | Device-specific Parameter 2 | ||||||
3 | 104 | 8-bit UInteger | Device-specific Parameter 3 | ||||||
4 | 96 | 8-bit UInteger | Device-specific Parameter 4 | ||||||
5 | 88 | 8-bit UInteger | Device-specific Parameter 5 | ||||||
6 | 80 | 8-bit UInteger | Device-specific Parameter 6 | ||||||
7 | 72 | 8-bit UInteger | Device-specific Parameter 7 | ||||||
8 | 64 | 8-bit UInteger | Device-specific Parameter 8 | ||||||
9 | 56 | 8-bit UInteger | Device-specific Parameter 9 | ||||||
10 | 48 | 8-bit UInteger | Device-specific Parameter 10 | ||||||
11 | 40 | 8-bit UInteger | Device-specific Parameter 11 | ||||||
12 | 32 | 8-bit UInteger | Device-specific Parameter 12 | ||||||
13 | 24 | 8-bit UInteger | Device-specific Parameter 13 | ||||||
14 | 16 | 8-bit UInteger | Device-specific Parameter 14 | ||||||
15 | 8 | 8-bit UInteger | Device-specific Parameter 15 | ||||||
16 | 0 | 8-bit UInteger | Device-specific Parameter 16 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
subindex | 1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 |
element bit | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 9 | 10 | 11 | 12 | 13 | 14 | 15 | 16 |
element bit | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 |
octet | 0 | |||||||
bit offset | 7 - 0 | |||||||
element bit | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 0 | Boolean | false = Unlocked, true = Locked | Parameter Write Access | This lock prevents the write access to all read/write parameters of the device except for the parameter 'Device Access Locks'. | ||||
2 | 1 | Boolean | false = Unlocked, true = Locked | false | Data Storage | This lock prevents the write access to the device parameters via the data storage mechanism. | |||
3 | 2 | Boolean | false = Unlocked, true = Locked | Local Parameterization | This lock prevents the device settings from being changed via local operating elements on the device. | ||||
4 | 3 | Boolean | false = Unlocked, true = Locked | Local User Interface | This lock prevents the access to the device settings and display via a local user interface. The user interface is disabled. |
bit offset | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
subindex | / / / / / / | / / / / / / | / / / / / / | / / / / / / | / / / / / / | / / / / / / | / / / / / / | / / / / / / |
bit offset | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
subindex | / / / / / / | / / / / / / | / / / / / / | / / / / / / | 4 | 3 | 2 | 1 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 407 - 400 | 399 - 392 | 391 - 384 | 383 - 376 | 375 - 368 | 367 - 360 | 359 - 352 | 351 - 344 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 343 - 336 | 335 - 328 | 327 - 320 | 319 - 312 | 311 - 304 | 303 - 296 | 295 - 288 | 287 - 280 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 279 - 272 | 271 - 264 | 263 - 256 | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 215 - 208 | 207 - 200 | 199 - 192 | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 |
octet | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 |
bit offset | 151 - 144 | 143 - 136 | 135 - 128 | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 |
octet | 40 | 41 | 42 | 43 | 44 | 45 | 46 | 47 |
bit offset | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 |
octet | 48 | 49 | 50 | |||||
bit offset | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 511 - 504 | 503 - 496 | 495 - 488 | 487 - 480 | 479 - 472 | 471 - 464 | 463 - 456 | 455 - 448 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 447 - 440 | 439 - 432 | 431 - 424 | 423 - 416 | 415 - 408 | 407 - 400 | 399 - 392 | 391 - 384 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 383 - 376 | 375 - 368 | 367 - 360 | 359 - 352 | 351 - 344 | 343 - 336 | 335 - 328 | 327 - 320 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 319 - 312 | 311 - 304 | 303 - 296 | 295 - 288 | 287 - 280 | 279 - 272 | 271 - 264 | 263 - 256 |
octet | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 |
bit offset | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 |
octet | 40 | 41 | 42 | 43 | 44 | 45 | 46 | 47 |
bit offset | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 |
octet | 48 | 49 | 50 | 51 | 52 | 53 | 54 | 55 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
octet | 56 | 57 | 58 | 59 | 60 | 61 | 62 | 63 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | |
bit offset | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | |||
bit offset | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 |
octet | 8 | 9 | 10 | |||||
bit offset | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | |||||||
bit offset | 7 - 0 | |||||||
element bit | 7 - 0 |
octet | 0 | 1 | 2 | |||||
bit offset | 23 - 16 | 15 - 8 | 7 - 0 | |||||
subindex | 1 | 1 | 1 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | |||||||
bit offset | 7 - 0 | |||||||
element bit | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 0 | 4-bit UInteger | 0 = Idle, 1 = Success SP1, 2 = Success SP2, 3 = Success SP1 and 2, 4 = Waiting for Command, 5 = Busy, 7 = Error | 0 | State | Shows the teach status of the teach-in process | |||
2 | 4 | Boolean | false = Not Taught, true = Taught | false | Teach Flag SP1 | Shows the teach status of the respective switch point | |||
4 | 6 | Boolean | false = Not Taught, true = Taught | false | Teach Flag SP2 | Shows the teach status of the respective switch point |
bit offset | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
subindex | / / / / / / | 4 | / / / / / / | 2 | 1 | |||
element bit | 3 | 2 | 1 | 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 32 | 32-bit Integer | 15000..530000 | 500000 | SP 1 | Set the distance at which the related SSC is set to active (or inactive if inverted) | |||
2 | 0 | 32-bit Integer | 15000..530000 | 15000 | SP 2 | Set the distance at which the related SSC is set to inactive (or active if inverted). Only active if SSC is set to window mode |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 1 | 1 | 1 | 1 | 2 | 2 | 2 | 2 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 24 | 8-bit UInteger | 0 = Normal, 1 = Inverted | 0 | Logic | Selects the SSC logic. It can be changed between 'active if object is present (normal)' or 'inactive if object is present (inverted)' | |||
2 | 16 | 8-bit UInteger | 0 = Disabled, 1 = Single Point, 2 = Window | 1 | Mode | Selects the SSC switch mode | |||
3 | 0 | 16-bit UInteger | 1 = Left Aligned, 2 = Center Aligned, 3 = Right Aligned | 3 | Hyst | Selects the hysteresis alignment mode |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 1 | 2 | 3 | 3 | ||||
element bit | 7 - 0 | 7 - 0 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 32 | 32-bit Integer | 15000..530000 | 500000 | SP 1 | Set the distance at which the related SSC is set to active (or inactive if inverted) | |||
2 | 0 | 32-bit Integer | 15000..530000 | 15000 | SP 2 | Set the distance at which the related SSC is set to inactive (or active if inverted). Only active if SSC is set to window mode |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 1 | 1 | 1 | 1 | 2 | 2 | 2 | 2 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 24 | 8-bit UInteger | 0 = Normal, 1 = Inverted | 0 | Logic | Selects the SSC logic. It can be changed between 'active if object is present (normal)' or 'inactive if object is present (inverted)' | |||
2 | 16 | 8-bit UInteger | 0 = Disabled, 1 = Single Point, 2 = Window | 1 | Mode | Selects the SSC switch mode | |||
3 | 0 | 16-bit UInteger | 1 = Left Aligned, 2 = Center Aligned, 3 = Right Aligned | 3 | Hyst | Selects the hysteresis alignment mode |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 1 | 2 | 3 | 3 | ||||
element bit | 7 - 0 | 7 - 0 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 0 | 16-bit UInteger | Value | Quality value indicates the quality of the reflected signal |
octet | 0 | 1 | ||||||
bit offset | 15 - 8 | 7 - 0 | ||||||
subindex | 1 | 1 | ||||||
element bit | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 0 | 16-bit UInteger | 0..400 | 120 | Threshold | Selects the Quality Threshold, if the quality value is below the threshold the LEDs start to blink and the quality bit in the process data is set to 1 |
octet | 0 | 1 | ||||||
bit offset | 15 - 8 | 7 - 0 | ||||||
subindex | 1 | 1 | ||||||
element bit | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 32 | 32-bit UInteger | 0..99 | 4 | SSC.1 Width | Adjust hysteresis width as percent of the switch point distance | |||
11 | 0 | 32-bit UInteger | 0..99 | 4 | SSC.2 Width | Adjust hysteresis width as percent of the switch point distance |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 1 | 1 | 1 | 1 | 11 | 11 | 11 | 11 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 16 | 16-bit UInteger | 1001 = Celsius | 1001 | Temperature | Select temperature unit (rw parameter in menu Parameter/ Temperature Settings, ro in menu Diagnosis/ Temperature internal) | |||
2 | 0 | 16-bit UInteger | 1054 = Second, 1058 = Minute, 1059 = Hour | 1054 | Time | Select time unit (rw parameter in menu Parameter/ Temperature Settings, ro in menu Diagnosis/ Operating Time) |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 1 | 1 | 2 | 2 | ||||
element bit | 15 - 8 | 7 - 0 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 56 | 8-bit UInteger | 1 = Push-Pull | 1 | OUT1 Circuit | Select the output function | |||
2 | 40 | 16-bit UInteger | 100 = SSC1, 200 = SSC2, 400 = SSC4 | 100 | OUT1 Mode | Select the SSC channel that is shown on the Pin | |||
13 | 0 | 16-bit UInteger | 0 = None | 0 | Input Mode | Select the function of the Input Pin |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 1 | 2 | 2 | / / / / / / | / / / / / / | / / / / / / | 13 | 13 |
element bit | 7 - 0 | 15 - 8 | 7 - 0 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 24 | 8-bit UInteger | 0 = Off, 1 = On | 1 | Green Mode | Switches the LED off, no change of other function | |||
12 | 16 | 8-bit UInteger | 0 = Off, 1 = On, 2 = Inverted | 1 | Yellow Mode | Switches the LED off, no change of other function, or inverts the relationship between LED and pin, Inverted: Pin high, LED off, On: Pin high, LED on | |||
22 | 8 | 8-bit UInteger | 0 = Off, 1 = On, 2 = Inverted | 0 | Red Mode | Switches the LED off, no change of other function, or inverts the relationship between LED and pin, Inverted: Pin high, LED off, On: Pin high, LED on | |||
32 | 0 | 8-bit UInteger | 0 = Off, 1 = On | 1 | Blue Mode | Switches the LED off, no change of other function |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 2 | 12 | 22 | 32 | ||||
element bit | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 0 | 8-bit UInteger | 0..120 | 5 | Teach Time Out | Time until Teach is locked. If 0 Teach never locks. If 0xFF Teach always off |
octet | 0 | |||||||
bit offset | 7 - 0 | |||||||
subindex | 1 | |||||||
element bit | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
31 | 8 | 8-bit UInteger | 2 = SSC.1 Switch Counter, 3 = SSC.2 Switch Counter | 2 | SSC.4 Selection | Select the switch counter that is used as input of SSC4 | |||
32 | 0 | 8-bit UInteger | 0 = Disabled, 2 = Enabled | 2 | SSC.4 Auto Reset | Auto Reset of switch counter if value in SSC.4 Param.SP1 is reached |
octet | 0 | 1 | ||||||
bit offset | 15 - 8 | 7 - 0 | ||||||
subindex | 31 | 32 | ||||||
element bit | 7 - 0 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 0 | 32-bit Integer | Distance | Measured distance |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 1 | 1 | 1 | 1 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 32 | 8-bit UInteger | 0 = Internal Temperature, 1 = External Temperature | 0 | Enable Environment Temperature | Enable usage of external environment temperature | |||
2 | 0 | Float32 | -40.05..84.85 | 20 | Environment Temperature | Sets the temperature that is used by sensor to calculate the distance. It is only used when the parameter 'Temperature Settings.Enable Environment temperature' is set to External Temperature. |
octet | 0 | 1 | 2 | 3 | 4 | |||
bit offset | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | |||
subindex | 1 | 2 | 2 | 2 | 2 | |||
element bit | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 64 | 32-bit UInteger | 0..60000 | 0 | SSC.1 Time | Sets / indicates the On delay switching output time in milliseconds for the respective switching signal channel (SSC). | |||
12 | 32 | 32-bit UInteger | 0..60000 | 0 | SSC.2 Time | Sets / indicates the On delay switching output time in milliseconds for the respective switching signal channel (SSC). | |||
32 | 0 | 32-bit UInteger | 0..60000 | 0 | SSC.4 Time | Sets / indicates the On delay switching output time in milliseconds for the respective switching signal channel (SSC). |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 2 | 2 | 2 | 2 | 12 | 12 | 12 | 12 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 32 | 32 | 32 | 32 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 64 | 32-bit UInteger | 0..60000 | 0 | SSC.1 Time | Sets / indicates the Off delay switching output time in milliseconds for the respective switching signal channel (SSC). | |||
12 | 32 | 32-bit UInteger | 0..60000 | 0 | SSC.2 Time | Sets / indicates the Off delay switching output time in milliseconds for the respective switching signal channel (SSC). | |||
32 | 0 | 32-bit UInteger | 0..60000 | 0 | SSC.4 Time | Sets / indicates the Off delay switching output time in milliseconds for the respective switching signal channel (SSC). |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 2 | 2 | 2 | 2 | 12 | 12 | 12 | 12 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 32 | 32 | 32 | 32 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 88 | 32-bit UInteger | 0..60000 | 0 | SSC.1 Time | Sets / indicates the minimal pulse length in milliseconds for the respective switching signal channel (SSC). | |||
3 | 80 | 8-bit UInteger | 1 = Both Pulses, 2 = Positive Pulse, 3 = Negative Pulse | 1 | SSC.1 Mode | 1: Both Pulses: positive and negative pulses are prolonged; 2: Positive Pulse: only positive pulses are prolonged; 3: Negative Pulse: only negative pulses are prolonged | |||
12 | 48 | 32-bit UInteger | 0..60000 | 0 | SSC.2 Time | Sets / indicates the minimal pulse length in milliseconds for the respective switching signal channel (SSC). | |||
13 | 40 | 8-bit UInteger | 1 = Both Pulses, 2 = Positive Pulse, 3 = Negative Pulse | 1 | SSC.2 Mode | 1: Both Pulses: positive and negative pulses are prolonged; 2: Positive Pulse: only positive pulses are prolonged; 3: Negative Pulse: only negative pulses are prolonged | |||
32 | 8 | 32-bit UInteger | 0..60000 | 0 | SSC.4 Time | Sets / indicates the minimal pulse length in milliseconds for the respective switching signal channel (SSC). | |||
33 | 0 | 8-bit UInteger | 1 = Both Pulses, 2 = Positive Pulse, 3 = Negative Pulse | 1 | SSC.4 Mode | 1: Both Pulses: positive and negative pulses are prolonged; 2: Positive Pulse: only positive pulses are prolonged; 3: Negative Pulse: only negative pulses are prolonged |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 |
subindex | 2 | 2 | 2 | 2 | 3 | 12 | 12 | 12 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | |
bit offset | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | |
subindex | 12 | 13 | 32 | 32 | 32 | 32 | 33 | |
element bit | 7 - 0 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 0 | 16-bit UInteger | 8..800 | 8 | Length | Selects the length of the distance value average filter over which values are averaged, it does not affect the cycle time. |
octet | 0 | 1 | ||||||
bit offset | 15 - 8 | 7 - 0 | ||||||
subindex | 2 | 2 | ||||||
element bit | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 32 | 16-bit UInteger | 0..10000 | 24 | Maximum perturbation time | Duration (in units of time) until a signal (as defined in the parameter .Distance) becomes visible at the output. | |||
3 | 0 | 32-bit UInteger | 1000..1000000 | 50000 | Distance | Distance deviations from the current measured value which are ignored, if shorter than the period set by the parameter '.Maximum perturbation time'. |
octet | 0 | 1 | 2 | 3 | 4 | 5 | ||
bit offset | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||
subindex | 2 | 2 | 3 | 3 | 3 | 3 | ||
element bit | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 96 | 32-bit UInteger | 15000..530000 | 15000 | Distance@Analog Min | Set the distance value in mm at the minimum value of the analog output | |||
3 | 64 | 32-bit UInteger | 40..200 | 40 | AnalogMin | Set the minimum value of the analog output | |||
4 | 32 | 32-bit UInteger | 15000..530000 | 500000 | Distance@Analog Max | Set the distance value in mm at the maximum value of the analog output | |||
5 | 0 | 32-bit UInteger | 40..200 | 200 | AnalogMax | Set the maximum value of the analog output |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 |
subindex | 2 | 2 | 2 | 2 | 3 | 3 | 3 | 3 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 4 | 4 | 4 | 4 | 5 | 5 | 5 | 5 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 0 | 32-bit Integer | 0 = Idle, 1 = Success, 2 = Error | Status | Shows the status of the analog output teach-in process |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 2 | 2 | 2 | 2 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 128 | Float32 | 0.0 | Current | Internal temperature of the sensor | ||||
2 | 96 | Float32 | 0.0 | Resetable Min | Minimal measured internal temperature of the sensor (Resetable) | ||||
3 | 64 | Float32 | 0.0 | Resetable Max | Maximal measured internal temperature of the sensor (Resetable) | ||||
4 | 32 | Float32 | 0.0 | Lifetime Min | Minimal measured internal temperature of the sensor (Lifetime) | ||||
5 | 0 | Float32 | 0.0 | Lifetime Max | Maximal measured internal temperature of the sensor (Lifetime) |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 |
subindex | 1 | 1 | 1 | 1 | 2 | 2 | 2 | 2 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 3 | 3 | 3 | 3 | 4 | 4 | 4 | 4 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 16 | 17 | 18 | 19 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 5 | 5 | 5 | 5 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 128 | Float32 | 0.0 | Current | Current power supply voltage | ||||
2 | 96 | Float32 | 0.0 | Resetable Min | Minimal measured power supply voltage (Resetable by user command) | ||||
3 | 64 | Float32 | 0.0 | Resetable Max | Maximal measured power supply voltage (Resetable by user command) | ||||
4 | 32 | Float32 | 0.0 | Lifetime Min | Minimal measured power supply voltage over the complete lifetime | ||||
5 | 0 | Float32 | 0.0 | Lifetime Max | Maximal measured power supply voltage over the complete lifetime |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 |
subindex | 1 | 1 | 1 | 1 | 2 | 2 | 2 | 2 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 3 | 3 | 3 | 3 | 4 | 4 | 4 | 4 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 16 | 17 | 18 | 19 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 5 | 5 | 5 | 5 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 64 | 32-bit UInteger | 0 | Powerup | Operation time on power-up | ||||
2 | 32 | 32-bit UInteger | 0 | Resetable | Operation time (Resetable by user command) | ||||
3 | 0 | 32-bit UInteger | 0 | Lifetime | Lifetime operation time |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 1 | 1 | 1 | 1 | 2 | 2 | 2 | 2 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 3 | 3 | 3 | 3 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 0 | 32-bit UInteger | 0 | Lifetime | Total number of bootcycles over the complete lifetime |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 2 | 2 | 2 | 2 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
2 | 64 | 32-bit UInteger | 0 | SSC.1 Resetable | Total number of switch counts on SSC.1 (resetable by user command-> SSC.1 Switch Counts Reset) | ||||
12 | 32 | 32-bit UInteger | 0 | SSC.2 Resetable | Total number of switch counts on SSC.2 (resetable by user command-> SSC.2 Switch Counts Reset) | ||||
32 | 0 | 32-bit UInteger | 0 | SSC.4 Resetable | Total number of switch counts on SSC.4 (resetable by user command-> SSC.4 Switch Counts Reset) |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 2 | 2 | 2 | 2 | 12 | 12 | 12 | 12 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | 11 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 32 | 32 | 32 | 32 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 0 | 16-bit UInteger | 0 = Narrow, 1 = Medium, 2 = Wide | 1 | Sonic Cone Adjustment | Set the width of the sonic cone |
octet | 0 | 1 | ||||||
bit offset | 15 - 8 | 7 - 0 | ||||||
subindex | 1 | 1 | ||||||
element bit | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 904 | 8-bit UInteger | Mode | ||||||
2 | 888 | 16-bit UInteger | Unit | ||||||
3 | 856 | Float32 | Range Start | ||||||
4 | 824 | Float32 | Range End | ||||||
5 | 816 | 8-bit UInteger | Nbr of Samples | ||||||
6 | 808 | 8-bit UInteger | Threshold low | ||||||
7 | 800 | 8-bit UInteger | Threshold high | ||||||
11 | 0 | 100-octet OctetString | Data |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 911 - 904 | 903 - 896 | 895 - 888 | 887 - 880 | 879 - 872 | 871 - 864 | 863 - 856 | 855 - 848 |
subindex | 1 | 2 | 2 | 3 | 3 | 3 | 3 | 4 |
element bit | 7 - 0 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 847 - 840 | 839 - 832 | 831 - 824 | 823 - 816 | 815 - 808 | 807 - 800 | 799 - 792 | 791 - 784 |
subindex | 4 | 4 | 4 | 5 | 6 | 7 | 11 | 11 |
element bit | 23 - 16 | 15 - 8 | 7 - 0 | 7 - 0 | 7 - 0 | 7 - 0 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 783 - 776 | 775 - 768 | 767 - 760 | 759 - 752 | 751 - 744 | 743 - 736 | 735 - 728 | 727 - 720 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 719 - 712 | 711 - 704 | 703 - 696 | 695 - 688 | 687 - 680 | 679 - 672 | 671 - 664 | 663 - 656 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 |
bit offset | 655 - 648 | 647 - 640 | 639 - 632 | 631 - 624 | 623 - 616 | 615 - 608 | 607 - 600 | 599 - 592 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 40 | 41 | 42 | 43 | 44 | 45 | 46 | 47 |
bit offset | 591 - 584 | 583 - 576 | 575 - 568 | 567 - 560 | 559 - 552 | 551 - 544 | 543 - 536 | 535 - 528 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 48 | 49 | 50 | 51 | 52 | 53 | 54 | 55 |
bit offset | 527 - 520 | 519 - 512 | 511 - 504 | 503 - 496 | 495 - 488 | 487 - 480 | 479 - 472 | 471 - 464 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 56 | 57 | 58 | 59 | 60 | 61 | 62 | 63 |
bit offset | 463 - 456 | 455 - 448 | 447 - 440 | 439 - 432 | 431 - 424 | 423 - 416 | 415 - 408 | 407 - 400 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 64 | 65 | 66 | 67 | 68 | 69 | 70 | 71 |
bit offset | 399 - 392 | 391 - 384 | 383 - 376 | 375 - 368 | 367 - 360 | 359 - 352 | 351 - 344 | 343 - 336 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 72 | 73 | 74 | 75 | 76 | 77 | 78 | 79 |
bit offset | 335 - 328 | 327 - 320 | 319 - 312 | 311 - 304 | 303 - 296 | 295 - 288 | 287 - 280 | 279 - 272 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 80 | 81 | 82 | 83 | 84 | 85 | 86 | 87 |
bit offset | 271 - 264 | 263 - 256 | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 | 223 - 216 | 215 - 208 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 88 | 89 | 90 | 91 | 92 | 93 | 94 | 95 |
bit offset | 207 - 200 | 199 - 192 | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 | 159 - 152 | 151 - 144 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 96 | 97 | 98 | 99 | 100 | 101 | 102 | 103 |
bit offset | 143 - 136 | 135 - 128 | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 | 95 - 88 | 87 - 80 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 104 | 105 | 106 | 107 | 108 | 109 | 110 | 111 |
bit offset | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 |
subindex | 11 | 11 | 11 | 11 | 11 | 11 | 11 | 11 |
octet | 112 | 113 | ||||||
bit offset | 15 - 8 | 7 - 0 | ||||||
subindex | 11 | 11 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 600 | 8-bit UInteger | Mode | Mode | |||||
2 | 584 | 16-bit UInteger | 1010 = Meter, 1011 = Kilometer, 1012 = Centimeter, 1013 = Millimeter, 1014 = Micrometer, 1997 = None | Unit | Unit | ||||
3 | 552 | Float32 | Range Start | Start of range | |||||
4 | 520 | Float32 | Range End | End of range | |||||
5 | 512 | 8-bit UInteger | Nbr of Bins | Number of acquired bins | |||||
11 | 480 | 32-bit UInteger | Bin 1 | Bin 1 | |||||
12 | 448 | 32-bit UInteger | Bin 2 | Bin 2 | |||||
13 | 416 | 32-bit UInteger | Bin 3 | Bin 3 | |||||
14 | 384 | 32-bit UInteger | Bin 4 | Bin 4 | |||||
15 | 352 | 32-bit UInteger | Bin 5 | Bin 5 | |||||
16 | 320 | 32-bit UInteger | Bin 6 | Bin 6 | |||||
17 | 288 | 32-bit UInteger | Bin 7 | Bin 7 | |||||
18 | 256 | 32-bit UInteger | Bin 8 | Bin 8 | |||||
19 | 224 | 32-bit UInteger | Bin 9 | Bin 9 | |||||
20 | 192 | 32-bit UInteger | Bin 10 | Bin 10 | |||||
21 | 160 | 32-bit UInteger | Bin 11 | Bin 11 | |||||
22 | 128 | 32-bit UInteger | Bin 12 | Bin 12 | |||||
23 | 96 | 32-bit UInteger | Bin 13 | Bin 13 | |||||
24 | 64 | 32-bit UInteger | Bin 14 | Bin 14 | |||||
25 | 32 | 32-bit UInteger | Bin 15 | Bin 15 | |||||
26 | 0 | 32-bit UInteger | Bin 16 | Bin 16 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 607 - 600 | 599 - 592 | 591 - 584 | 583 - 576 | 575 - 568 | 567 - 560 | 559 - 552 | 551 - 544 |
subindex | 1 | 2 | 2 | 3 | 3 | 3 | 3 | 4 |
element bit | 7 - 0 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 543 - 536 | 535 - 528 | 527 - 520 | 519 - 512 | 511 - 504 | 503 - 496 | 495 - 488 | 487 - 480 |
subindex | 4 | 4 | 4 | 5 | 11 | 11 | 11 | 11 |
element bit | 23 - 16 | 15 - 8 | 7 - 0 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 479 - 472 | 471 - 464 | 463 - 456 | 455 - 448 | 447 - 440 | 439 - 432 | 431 - 424 | 423 - 416 |
subindex | 12 | 12 | 12 | 12 | 13 | 13 | 13 | 13 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 415 - 408 | 407 - 400 | 399 - 392 | 391 - 384 | 383 - 376 | 375 - 368 | 367 - 360 | 359 - 352 |
subindex | 14 | 14 | 14 | 14 | 15 | 15 | 15 | 15 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 |
bit offset | 351 - 344 | 343 - 336 | 335 - 328 | 327 - 320 | 319 - 312 | 311 - 304 | 303 - 296 | 295 - 288 |
subindex | 16 | 16 | 16 | 16 | 17 | 17 | 17 | 17 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 40 | 41 | 42 | 43 | 44 | 45 | 46 | 47 |
bit offset | 287 - 280 | 279 - 272 | 271 - 264 | 263 - 256 | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 |
subindex | 18 | 18 | 18 | 18 | 19 | 19 | 19 | 19 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 48 | 49 | 50 | 51 | 52 | 53 | 54 | 55 |
bit offset | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 |
subindex | 20 | 20 | 20 | 20 | 21 | 21 | 21 | 21 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 56 | 57 | 58 | 59 | 60 | 61 | 62 | 63 |
bit offset | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 |
subindex | 22 | 22 | 22 | 22 | 23 | 23 | 23 | 23 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 64 | 65 | 66 | 67 | 68 | 69 | 70 | 71 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 24 | 24 | 24 | 24 | 25 | 25 | 25 | 25 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 72 | 73 | 74 | 75 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 26 | 26 | 26 | 26 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 600 | 8-bit UInteger | Mode | Mode | |||||
2 | 584 | 16-bit UInteger | 1240 = Volt, 1243 = Millivolt | Unit | Unit | ||||
3 | 552 | Float32 | Range Start | Start of range | |||||
4 | 520 | Float32 | Range End | End of range | |||||
5 | 512 | 8-bit UInteger | Nbr of Bins | Number of acquired bins | |||||
11 | 480 | 32-bit UInteger | Bin 1 | Bin 1 | |||||
12 | 448 | 32-bit UInteger | Bin 2 | Bin 2 | |||||
13 | 416 | 32-bit UInteger | Bin 3 | Bin 3 | |||||
14 | 384 | 32-bit UInteger | Bin 4 | Bin 4 | |||||
15 | 352 | 32-bit UInteger | Bin 5 | Bin 5 | |||||
16 | 320 | 32-bit UInteger | Bin 6 | Bin 6 | |||||
17 | 288 | 32-bit UInteger | Bin 7 | Bin 7 | |||||
18 | 256 | 32-bit UInteger | Bin 8 | Bin 8 | |||||
19 | 224 | 32-bit UInteger | Bin 9 | Bin 9 | |||||
20 | 192 | 32-bit UInteger | Bin 10 | Bin 10 | |||||
21 | 160 | 32-bit UInteger | Bin 11 | Bin 11 | |||||
22 | 128 | 32-bit UInteger | Bin 12 | Bin 12 | |||||
23 | 96 | 32-bit UInteger | Bin 13 | Bin 13 | |||||
24 | 64 | 32-bit UInteger | Bin 14 | Bin 14 | |||||
25 | 32 | 32-bit UInteger | Bin 15 | Bin 15 | |||||
26 | 0 | 32-bit UInteger | Bin 16 | Bin 16 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 607 - 600 | 599 - 592 | 591 - 584 | 583 - 576 | 575 - 568 | 567 - 560 | 559 - 552 | 551 - 544 |
subindex | 1 | 2 | 2 | 3 | 3 | 3 | 3 | 4 |
element bit | 7 - 0 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 543 - 536 | 535 - 528 | 527 - 520 | 519 - 512 | 511 - 504 | 503 - 496 | 495 - 488 | 487 - 480 |
subindex | 4 | 4 | 4 | 5 | 11 | 11 | 11 | 11 |
element bit | 23 - 16 | 15 - 8 | 7 - 0 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 479 - 472 | 471 - 464 | 463 - 456 | 455 - 448 | 447 - 440 | 439 - 432 | 431 - 424 | 423 - 416 |
subindex | 12 | 12 | 12 | 12 | 13 | 13 | 13 | 13 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 415 - 408 | 407 - 400 | 399 - 392 | 391 - 384 | 383 - 376 | 375 - 368 | 367 - 360 | 359 - 352 |
subindex | 14 | 14 | 14 | 14 | 15 | 15 | 15 | 15 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 |
bit offset | 351 - 344 | 343 - 336 | 335 - 328 | 327 - 320 | 319 - 312 | 311 - 304 | 303 - 296 | 295 - 288 |
subindex | 16 | 16 | 16 | 16 | 17 | 17 | 17 | 17 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 40 | 41 | 42 | 43 | 44 | 45 | 46 | 47 |
bit offset | 287 - 280 | 279 - 272 | 271 - 264 | 263 - 256 | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 |
subindex | 18 | 18 | 18 | 18 | 19 | 19 | 19 | 19 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 48 | 49 | 50 | 51 | 52 | 53 | 54 | 55 |
bit offset | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 |
subindex | 20 | 20 | 20 | 20 | 21 | 21 | 21 | 21 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 56 | 57 | 58 | 59 | 60 | 61 | 62 | 63 |
bit offset | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 |
subindex | 22 | 22 | 22 | 22 | 23 | 23 | 23 | 23 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 64 | 65 | 66 | 67 | 68 | 69 | 70 | 71 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 24 | 24 | 24 | 24 | 25 | 25 | 25 | 25 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 72 | 73 | 74 | 75 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 26 | 26 | 26 | 26 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 600 | 8-bit UInteger | Mode | Mode | |||||
2 | 584 | 16-bit UInteger | 1001 = Celsius | Unit | Unit | ||||
3 | 552 | Float32 | Range Start | Start of range | |||||
4 | 520 | Float32 | Range End | End of range | |||||
5 | 512 | 8-bit UInteger | Nbr of Bins | Number of acquired bins | |||||
11 | 480 | 32-bit UInteger | Bin 1 | Bin 1 | |||||
12 | 448 | 32-bit UInteger | Bin 2 | Bin 2 | |||||
13 | 416 | 32-bit UInteger | Bin 3 | Bin 3 | |||||
14 | 384 | 32-bit UInteger | Bin 4 | Bin 4 | |||||
15 | 352 | 32-bit UInteger | Bin 5 | Bin 5 | |||||
16 | 320 | 32-bit UInteger | Bin 6 | Bin 6 | |||||
17 | 288 | 32-bit UInteger | Bin 7 | Bin 7 | |||||
18 | 256 | 32-bit UInteger | Bin 8 | Bin 8 | |||||
19 | 224 | 32-bit UInteger | Bin 9 | Bin 9 | |||||
20 | 192 | 32-bit UInteger | Bin 10 | Bin 10 | |||||
21 | 160 | 32-bit UInteger | Bin 11 | Bin 11 | |||||
22 | 128 | 32-bit UInteger | Bin 12 | Bin 12 | |||||
23 | 96 | 32-bit UInteger | Bin 13 | Bin 13 | |||||
24 | 64 | 32-bit UInteger | Bin 14 | Bin 14 | |||||
25 | 32 | 32-bit UInteger | Bin 15 | Bin 15 | |||||
26 | 0 | 32-bit UInteger | Bin 16 | Bin 16 |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 607 - 600 | 599 - 592 | 591 - 584 | 583 - 576 | 575 - 568 | 567 - 560 | 559 - 552 | 551 - 544 |
subindex | 1 | 2 | 2 | 3 | 3 | 3 | 3 | 4 |
element bit | 7 - 0 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 |
octet | 8 | 9 | 10 | 11 | 12 | 13 | 14 | 15 |
bit offset | 543 - 536 | 535 - 528 | 527 - 520 | 519 - 512 | 511 - 504 | 503 - 496 | 495 - 488 | 487 - 480 |
subindex | 4 | 4 | 4 | 5 | 11 | 11 | 11 | 11 |
element bit | 23 - 16 | 15 - 8 | 7 - 0 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 16 | 17 | 18 | 19 | 20 | 21 | 22 | 23 |
bit offset | 479 - 472 | 471 - 464 | 463 - 456 | 455 - 448 | 447 - 440 | 439 - 432 | 431 - 424 | 423 - 416 |
subindex | 12 | 12 | 12 | 12 | 13 | 13 | 13 | 13 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 24 | 25 | 26 | 27 | 28 | 29 | 30 | 31 |
bit offset | 415 - 408 | 407 - 400 | 399 - 392 | 391 - 384 | 383 - 376 | 375 - 368 | 367 - 360 | 359 - 352 |
subindex | 14 | 14 | 14 | 14 | 15 | 15 | 15 | 15 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 32 | 33 | 34 | 35 | 36 | 37 | 38 | 39 |
bit offset | 351 - 344 | 343 - 336 | 335 - 328 | 327 - 320 | 319 - 312 | 311 - 304 | 303 - 296 | 295 - 288 |
subindex | 16 | 16 | 16 | 16 | 17 | 17 | 17 | 17 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 40 | 41 | 42 | 43 | 44 | 45 | 46 | 47 |
bit offset | 287 - 280 | 279 - 272 | 271 - 264 | 263 - 256 | 255 - 248 | 247 - 240 | 239 - 232 | 231 - 224 |
subindex | 18 | 18 | 18 | 18 | 19 | 19 | 19 | 19 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 48 | 49 | 50 | 51 | 52 | 53 | 54 | 55 |
bit offset | 223 - 216 | 215 - 208 | 207 - 200 | 199 - 192 | 191 - 184 | 183 - 176 | 175 - 168 | 167 - 160 |
subindex | 20 | 20 | 20 | 20 | 21 | 21 | 21 | 21 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 56 | 57 | 58 | 59 | 60 | 61 | 62 | 63 |
bit offset | 159 - 152 | 151 - 144 | 143 - 136 | 135 - 128 | 127 - 120 | 119 - 112 | 111 - 104 | 103 - 96 |
subindex | 22 | 22 | 22 | 22 | 23 | 23 | 23 | 23 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 64 | 65 | 66 | 67 | 68 | 69 | 70 | 71 |
bit offset | 95 - 88 | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 |
subindex | 24 | 24 | 24 | 24 | 25 | 25 | 25 | 25 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 72 | 73 | 74 | 75 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
subindex | 26 | 26 | 26 | 26 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 0 | 1 | 2 | 3 | ||||
bit offset | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | ||||
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 32 | 32-bit Integer | 0..2147483639 | 20 | SP 1 | Set the number of counts at which the SSC is set to active (or inactive if inverted) | |||
2 | 0 | 32-bit Integer | 0..2147483639 | 0 | SP 2 | Set the number of counts at which the SSC is set to inactive (or active if inverted). Only active if SSC is set to window mode |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | 1 | 1 | 1 | 1 | 2 | 2 | 2 | 2 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 8 | 8-bit UInteger | 0 = Normal, 1 = Inverted | 0 | Logic | Selects the SSC logic. It can be changed between active if object is present (normal) or inactive if object is present (inverted) | |||
2 | 0 | 8-bit UInteger | 0 = Disabled, 1 = Single Point, 2 = Window | 0 | Mode | Selection of the switching mode |
octet | 0 | 1 | ||||||
bit offset | 15 - 8 | 7 - 0 | ||||||
subindex | 1 | 2 | ||||||
element bit | 7 - 0 | 7 - 0 |
subindex | bit offset | data type | allowed values | default value | acc. restr. | mod. other var. | excl. from DS | name | description |
---|---|---|---|---|---|---|---|---|---|
1 | 56 | 32-bit Integer | 15000 | Lower Limit | Lower value of measuring range, if value is below out of range is shown | ||||
2 | 24 | 32-bit Integer | 530000 | Upper Limit | Upper value of measuring range, if value is above out of range is shown | ||||
3 | 8 | 16-bit UInteger | 1010 = Meter, 1011 = Kilometer, 1012 = Centimeter, 1013 = Millimeter, 1014 = Micrometer, 1997 = None | 1010 | Unit Code | Indicates the unit of the selected MDC source | |||
4 | 0 | 8-bit Integer | -6 | Scale | Value of the exponent to the base of ten, applicable to the value of the MDC |
octet | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
bit offset | 87 - 80 | 79 - 72 | 71 - 64 | 63 - 56 | 55 - 48 | 47 - 40 | 39 - 32 | 31 - 24 |
subindex | 1 | 1 | 1 | 1 | 2 | 2 | 2 | 2 |
element bit | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 | 31 - 24 | 23 - 16 | 15 - 8 | 7 - 0 |
octet | 8 | 9 | 10 | |||||
bit offset | 23 - 16 | 15 - 8 | 7 - 0 | |||||
subindex | 3 | 3 | 4 | |||||
element bit | 15 - 8 | 7 - 0 | 7 - 0 |
Formatting for Process Data id=PI_ProcessDataIn |
---|
Subindex 1: * 0.001 + 0 mm Dec.3 |
Subindex 2: |
Subindex 5: |
Subindex 7: |
Subindex 8: |
Subindex 9: |
Subindex 10: |
Formatting for Process Data id=PO_ProcessDataOut |
---|
Subindex 1: |
Subindex 2: |
Subindex 3: |
Identification Menu |
---|
V_VendorName |
V_VendorText |
V_ProductName |
V_ProductID |
V_ProductText |
V_ApplicationSpecificTag |
V_FunctionTag |
V_LocationTag |
V_SerialNumber |
V_FirmwareRevision |
V_HardwareRevision |
Identification Menu |
---|
V_VendorName |
V_VendorText |
V_ProductName |
V_ProductID |
V_ProductText |
V_ApplicationSpecificTag |
V_FunctionTag |
V_LocationTag |
V_SerialNumber |
V_FirmwareRevision |
V_HardwareRevision |
Parameters Menu | |||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
|
Diagnosis Menu | ||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
V_DeviceStatus | ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
|
Identification Menu |
---|
V_VendorName |
V_VendorText |
V_ProductName |
V_ProductID |
V_ProductText |
V_ApplicationSpecificTag |
V_FunctionTag |
V_LocationTag |
V_SerialNumber |
V_FirmwareRevision |
V_HardwareRevision |
Parameters Menu | |||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
| |||||||||||||||||
|
Diagnosis Menu | ||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
V_DeviceStatus | ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
| ||||||||||||||
|
Note: This page shows the content of an IODD file transformed into HTML format. In the case of disparity between this and the XML view, the content of the XML file takes precedence.
Created by IODD Viewer V1.4.